Disable the SGI.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disable the SGI.

Jump to solution
5,353 Views
takashitakahash
Contributor III

Hi community.

Our customer would like to disable the SGI.

In the current Integrity OS, SGI( Software-generated Interrupts) is enabled by default.

For SGI is not used in customer system, we want to disable.

Would you advice should be disabled in any such a procedure?

If you have any sample software I think want me to reference.

Labels (1)
0 Kudos
Reply
1 Solution
4,972 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
5 Replies
4,973 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
4,974 Views
takashitakahash
Contributor III


Hello Jiri-san

Thank you for your information.

I talk to with taku-sann GIC settings.

Thank you,

Best.

T.Takahashi.

4,974 Views
rendy
NXP Employee
NXP Employee

Hi,

this looks like a question for Green Hills (developer of INTEGRITY RTOS).

Regards

Rene

0 Kudos
Reply
4,974 Views
karina_valencia
NXP Apps Support
NXP Apps Support

rendy​ what is the next step here?

0 Kudos
Reply
4,974 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

this has  been discussed with Taku-san. It is depended on design of SoC (based on implementation or ARM GIC). It is not possible to disable SGI separately.

You can

- disable all interrupts or

- do not assert software interrupts

/Jiri

P.S. discussed internally here  Vybrid SGI implementation and SGI configuration on Vybrid