DCU operating modes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,620件の閲覧回数
falstaff
Senior Contributor I

Hi,

Internal tests have shown different operating modes being used than documented. The Reference Manual Rev. 7 states for the field DCU_MODE in DCUx_DCU_MODE register:

DCU operating mode

00

DCU off (pixel clock active if enabled by I/O).
01Normal mode. Panel content controlled by layer configuration.
10

Test mode. DCU disables all DMA fetches and all the pixels of an enabled layer take the value in the

CLUT RAM selected by the respective LUOFFS field of control descriptor 4.

11Color Bar Generation. Panel content controlled by color bar registers.

Hence, clearing the DCU_MODE register using something like DCU_MODE & ~0x3 should turn off the DCU controller, however tests on MVF61 and MVF50 parts have shown that when clearing the DCU_MODE field, the DCU controller seems to enter the test mode. However, when using 0x2, which should be the Test mode, the display stays off (hence this seems to be the DCU off mode).

Is this a documentation error? Can somebody confirm?

Best regards,

Stefan Agner

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
3,207件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Stefan,

I have tested in the MVF61GS which is found in the TWR system and the DCU MODE operation works as expected.

MASK set is 1N02G. Are your facing the same issue in the TWR system?

/Alejandro

元の投稿で解決策を見る

2 返答(返信)
3,208件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Stefan,

I have tested in the MVF61GS which is found in the TWR system and the DCU MODE operation works as expected.

MASK set is 1N02G. Are your facing the same issue in the TWR system?

/Alejandro

3,207件の閲覧回数
falstaff
Senior Contributor I

Hi Alejandro,

Sorry, you are right, DCU works as expected.

The DCU off mode left the pixel clock on as documented, which in turn enabled a test mode in my display! Without reading the exact description of the DCU test mode, I assumed that the test mode I saw is generated by DCU... However, when using the DCU test mode, the screen stayed black since I did not had any look up tables (LUOFFS) configured.

This lead me to the conclusion that the DCU operating modes were mixed up...

Sorry about the noise and thanks for verifying this.

--

Stefan

0 件の賞賛
返信