Clearing SNVS Interrupts

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Clearing SNVS Interrupts

跳至解决方案
3,525 次查看
ryanm_
Contributor II

Using the Vybrid Security Reference Manual (Rev 1, 5/2013) I've been able to write code to configure and setup SNVS for external and wire-mesh tamper events.  I'm able to force tamper and see the indicated in the SNVS_HPSVSR and SNVS_LPSR.

When I enable security violations and setup the interrupts via SNVS_HPSICR and force a tamper event an interrupt will be generated to my software.  How do I clear the SNVS security violation interrupts?  (I've tried writing 0xFFFFFFFF to SNVS_LPSR & SNVS_HPSVSR with no luck.

Thanks,

Ryan

标签 (1)
0 项奖励
回复
1 解答
2,770 次查看
ryanm_
Contributor II

I was already setting the register "SNVS_HPCOMR[NPSWA_EN] = 1"  and it did not fix the issue.  My work around to the issue was to unregister for the interrupt. 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,771 次查看
ryanm_
Contributor II

I was already setting the register "SNVS_HPCOMR[NPSWA_EN] = 1"  and it did not fix the issue.  My work around to the issue was to unregister for the interrupt. 

0 项奖励
回复
2,770 次查看
juangutierrez
NXP Employee
NXP Employee

My guess is that in order to be able to clear the status flag, you should first move to a non-secure mode or a soft-fail mode

I found some code, where they are checking that the state is soft-fail and caam is in state mode before clearing the violation. But not sure exactly where the state is really moved

The reg32_read_test, seems to be just reading and comparing against the expected value, but not really writing.

void snvs_sec_interrupt(void){

   reg32_read_tst(SNVS_HPSR,   0x80000300,0xFFFFFFFF); // Moved to Soft-Fail

   reg32_read_tst(CAAM_CSTA,   0x00000300,0x00000300); // CAAM in Fail Mode

   reg32_read_tst(SNVS_LPSR,   0x40000000,0xFFFFFFFF);

   reg32clrbit   (SNVS_HPCOMR, 9);                     // clr fail security violation

   // Probably move back to secure mode here

   return;

}

Hope you find this info useful

2,770 次查看
ryanm_
Contributor II

I tried adding the specified code to the interrupt handler to clear the interrupt and didn't have any luck with it clearing the interrupt. 

0 项奖励
回复
2,770 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

juangutierrez can you continue with the follow up?

0 项奖励
回复
2,770 次查看
juangutierrez
NXP Employee
NXP Employee

Privileged read/write accessible registers can only be accessed for read/write by privileged software. Unauthorized write accesses are ignored, and unauthorized read accesses return zero. Non-privileged software can access privileged access registers when the non-privileged software access enable bit is set in the SNVS _HP Command Register.

In addition, all privileged access registers (except HPSVSR and LPSR) can be written to only if the system security monitor is in one of the three functional states:

• Non-Secure

• Trusted

• Secure

So I guess you need to move to one of this states in order to be able to

Try to Enable SNVS_HPCOMR[NPSWA_EN], so any software can access privileged registers, and see it that helps

0 项奖励
回复
2,770 次查看
juangutierrez
NXP Employee
NXP Employee

Well, actually it says except for HPSVSR and LPSR

Hmm, anyway can you try enabling SNVS_HPCOMR[NPSWA_EN]

0 项奖励
回复