Blending layers.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,026件の閲覧回数
takashitakahash
Contributor III

Hi community.

Desclibe on Vybrid Reference Manual, Rev.5 of 55.2.2 Features below.

・Blending of each pixel using up to 6 source layers dependent on size of panel

Question1

Does this sense would up 6 Layers that it can be blending simultaneously.

Or simultaneous blending Will to 6 pixels.

If 6 pixels.

Question2

What is six upper limit of the overlap of the frame buffer.

And ,In the same coordinates on the transparency (alpha value fully transparent), NOCOUNT is pixel.

ラベル(1)
0 件の賞賛
返信
1 解決策
860件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I am not sure if I understand correctly the question. But you can blend up to 6 layers. And every pixel that overlaps to other will be taken care of.

Here you can find a training that explains the DCU module. In concept it applies to vybrid.

http://www.freescale.com/files/training/doc/dwf/DWF13_APF_AUT_T0500.pdf

I hope that helps.

/Alejandro

元の投稿で解決策を見る

1 返信
861件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I am not sure if I understand correctly the question. But you can blend up to 6 layers. And every pixel that overlaps to other will be taken care of.

Here you can find a training that explains the DCU module. In concept it applies to vybrid.

http://www.freescale.com/files/training/doc/dwf/DWF13_APF_AUT_T0500.pdf

I hope that helps.

/Alejandro