Binary Loading : TCM and OCRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Binary Loading : TCM and OCRAM

Jump to solution
3,574 Views
carlovalgocela
Contributor III

Hello

In Vybrid Architecture manual, a TCM backdoor is intended to load the code and data into TCM by Cortex-A5 (primary core) prior to running Cortex-M4 (secondary core).

It actual it is loaded in the OCRAM-SysRAM0.  Can anybody explain why it is loaded in SysRAM0 and not in the TCM?

Thanks

Labels (3)
Tags (3)
0 Kudos
Reply
1 Solution
3,191 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
3,192 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
3,194 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Carlo,

missing some information like which code or data, what project...

Anyway, generally the placement of the code and data depends on Linker command file (IAR) - see supp.iar.com or scatter file  (DS5) - see Loading this site

Depending on your IDE you can select location of your code and date and build the project with this setting. Then your code will be placed where you want.

/Jiri