About external 24MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,951件の閲覧回数
keisukewatanabe
Contributor III

Dear support,

We'd like to provide 24MHz from an external crystal osc.

In this case, should we provide the power for the crystal osc from VDD(1.2V)?

Or should we provide the power from DECAP_V11_LDO_OUT(1.1V)?

We can not determine one from reading the suggestion in the datasheet.

Best regards,

Keisuke

ラベル(1)
0 件の賞賛
返信
1 解決策
1,749件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Keisuke,

This issue has been already discussed here - https://community.freescale.com/thread/308168.

Regards, Naoum Gitnik.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,750件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Keisuke,

This issue has been already discussed here - https://community.freescale.com/thread/308168.

Regards, Naoum Gitnik.

0 件の賞賛
返信