Mail notification of file upload

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mail notification of file upload

4,604 Views
hiroshinoma
NXP Employee
NXP Employee

I am now running a private community.

One of the feature I am interested in using is a mail notification.

Would it be possible to activate this feature as soon as the file is upload into community and published?

If so, what will be the required setting(s) for a user who wants it?

Thanks!

0 Kudos
Reply
3 Replies

4,036 Views
dianatorres
NXP Employee
NXP Employee

Hi Hiroshi,

In order for members of your private community to be able to receive inbox notifications when a piece of content is either created, uploaded or modified, they must follow the space and select inbox check-mark.

pastedImage_0.png

Note: Users must follow this procedure for each space, group or project they want to receive notifications from.

Best regards,

Diana Torres

NXP Enterprise Community Manager

0 Kudos
Reply

4,036 Views
hiroshinoma
NXP Employee
NXP Employee

Hi Diana,

This method worked for me, but not for a member in the community.

We have tested further and here is what we found:

-Notification after posting from the top page of the community was successful.

-Notification after uploading a file from the project page(USB Type-C) was unsuccessful.

Some screen shots for reference.

Any idea?

Best Regards,

Hiroshi Noma

Senior Engineer

Security & Connectivity

Application Engineering Department

Customer Application Engineering Division

NXP Semiconductors Japan Ltd

Yebisu Garden Place Tower 24F

4-20-3 Ebisu, Shibuya-ku, Tokyo 150-6024 JAPAN

TEL: +81-3-6732-7867, FAX: +81-3-6732-7947

E-mail: hiroshi.noma@nxp.com<mailto:keiko.irie@nxp.com> URL: www.nxp.com<http://www.nxp.com/>;

0 Kudos
Reply

4,036 Views
aravinthkumarja
Senior Contributor II

Hi Hiroshi Noma,

=> Do you have private community in freescale or others..?

=> Every reply notification you can get through mail also. but they won't split file uploaded reply's.

Regards,

Aravinth

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply