Connecting two flash in parallel using 32 bit data bus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting two flash in parallel using 32 bit data bus

1,512 Views
manjunathgangad
Contributor II

We have one design constraint to use two flash connected in parallel: First flash uses (D0-D15) and second flash uses D16 - D31. Using same physically address for both flash with available 28 bit address bus using A1 - A19. For example, When we write double word into flash, it is as good as writing first word into first flash and second word into second flash.

We need to know how to send commands to both flash at same time for operation like READ or WRITE. Both flash shares same CE, OE & WE.

Regards,

Manjunath

0 Kudos
Reply
0 Replies