project generator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

project generator

7,161 Views
zhangxiuli
Contributor I

project generator.exe can't open

Labels (2)
3 Replies

6,465 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello xiuli,

Which project generator.exe ?  The kinetis KSDK proeject generator ?

What about your system ?

Could you please describe it detail and show the error .

BR

Alice

0 Kudos
Reply

6,465 Views
zhangxiuli
Contributor I

Hello Alice,

I'm very glad to receive your reply.

Yes,  The KSDK_Proeject_Generator.exe can not open,my OS is win10.

When I try to open the KSDK_Proeject_Generator.exe,windows prompt a "Fatal Error",

and show "KSDK_Proeject_Generator.exe.manifest could not be extracted!".

picture follow

GMKC50BM4AGZ7`AJ_F8P4{3.png

thank you!

Best wishes,

xiuli

0 Kudos
Reply

6,465 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello xiuli,

Sorry for that  so far the KSDK project generator  only support these system :

pastedImage_0.png

we can find this on the DOC : KSDK Project Generator Release Notes - 2.0.pdf .

You can test it on other system , and i have test , it also can work on Windows 7 64 bit .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------