git.am.freescale.net connection error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

git.am.freescale.net connection error

3,985件の閲覧回数
srikanthkolla
Contributor I


I was installing Yocto for t1040 rdb board and when I tried "bitbake fsl-image-core", I got the following error:

Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/sdk/l2switch-util.git;branch=master'. Unable to fetch URL from any source.

WARNING: Failed to fetch URL git://git.am.freescale.net/gitolite/sdk/l2switch-util.git;branch=master, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/sirius/yocto/poky/build_t1040rdb_release/../sources/git2/git.am.freescale.net.gitolite.sdk.l2switch-util.git'...
fatal: unable to connect to git.am.freescale.net:
git.am.freescale.net: No address associated with hostname


ERROR: Function failed: Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/sdk/l2switch-util.git;branch=master'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/sirius/yocto/poky/build_t1040rdb_release/tmp/work/ppce5500-fsl-linux/l2switch/0.1-r0/temp/log.do_fetch.18404
ERROR: Task 662 (/home/sirius/yocto/meta-fsl-networking/recipes-extended/l2switch/l2switch_0.1.bb, do_fetch) failed with exit code '1'

What am I supposed to do now?

0 返答(返信)