UART ON MPC5606B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART ON MPC5606B

3,276 次查看
rogercovarrubia
Contributor III

Does anybody has an example or application note on how to use the UART on the MPC5606B???

Thanks

3 回复数

2,596 次查看
FlavioStiffan
NXP Employee
NXP Employee

2,596 次查看
michaelgoudey
NXP Employee
NXP Employee

Roger,

Did Flavio's response help you?  There is a zip file with example drivers associated with this App Note.  It configures LinFlex in UART mode.

     http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4850SW.zip?fpsp=1

You may also consider the PDF examples included for the TRK-USB-MPC5604B board.  It has simple LinFlex UART examples included in the PDF:

     http://cache.freescale.com/files/microcontrollers/doc/support_info/TRK-USB-MPC5604B_LAB.pdf

     http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TRK-USB-MPC5604B

Regards,

Michael Goudey

2,596 次查看
rogercovarrubia
Contributor III

Thanks Guys

0 项奖励
回复