Need help with MCU selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help with MCU selection

ソリューションへジャンプ
3,048件の閲覧回数
olajuwon
Contributor I

I'm working on my senior design project where I'm expected to build a PCB for a wearable device. We were shown an existing prototype that was built using the teensy 3.1 development board which host an MK20DX256 chip which has a 32 bit ARM Cortex-M4 (72 MHz). I was hoping to replace the current MCU with something  with a similar core and Bluetooth Low Energy transceiver. I was looking the chips in the k series but the drop-off in processor speed seems huge. If anyone can help give some direction.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,800件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

The Kinetis KW2 runs at 50Mhz and has a thinner package than the KW20 series, this allows a better footprint and a thinner overall application packaging. The change in clock speed must be compensated by a more efficient running code.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,801件の閲覧回数
FlavioStiffan
NXP Employee
NXP Employee

The Kinetis KW2 runs at 50Mhz and has a thinner package than the KW20 series, this allows a better footprint and a thinner overall application packaging. The change in clock speed must be compensated by a more efficient running code.

0 件の賞賛
返信