Need help with MCU selection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need help with MCU selection

Jump to solution
3,109 Views
olajuwon
Contributor I

I'm working on my senior design project where I'm expected to build a PCB for a wearable device. We were shown an existing prototype that was built using the teensy 3.1 development board which host an MK20DX256 chip which has a 32 bit ARM Cortex-M4 (72 MHz). I was hoping to replace the current MCU with something  with a similar core and Bluetooth Low Energy transceiver. I was looking the chips in the k series but the drop-off in processor speed seems huge. If anyone can help give some direction.

Labels (1)
0 Kudos
Reply
1 Solution
2,861 Views
FlavioStiffan
NXP Employee
NXP Employee

The Kinetis KW2 runs at 50Mhz and has a thinner package than the KW20 series, this allows a better footprint and a thinner overall application packaging. The change in clock speed must be compensated by a more efficient running code.

View solution in original post

0 Kudos
Reply
1 Reply
2,862 Views
FlavioStiffan
NXP Employee
NXP Employee

The Kinetis KW2 runs at 50Mhz and has a thinner package than the KW20 series, this allows a better footprint and a thinner overall application packaging. The change in clock speed must be compensated by a more efficient running code.

0 Kudos
Reply