Is it possible/wise to interface my Freedom board with my PBMCUSLK project boards?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is it possible/wise to interface my Freedom board with my PBMCUSLK project boards?

1,432 次查看
davehaas
Contributor I

We are switching our course from the M52233DEMO board to the ARM Freedom board.  Is there a convenient way to interface our Project boards, PBMCUSLK, with the Freedom or do we start the interfacing from scratch?

Thanks

Dave Haas

NJIT

标签 (1)
0 项奖励
回复
1 回复

1,122 次查看
admin
Specialist II

Not directly via the MCU_PORT.  The Freescale Freedom boards outmost row follows the Arduino pin scheme which I am not sure if you can plug that into the breadboard surface.  I don't have the single row of pins to test it out.  (Double rows obviously would not work because you would be shorting two pins together.)

Are you using the NI-ELVIS board in combination with the PBMCUSLK?

~John

0 项奖励
回复