Is it possible/wise to interface my Freedom board with my PBMCUSLK project boards?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible/wise to interface my Freedom board with my PBMCUSLK project boards?

1,478 Views
davehaas
Contributor I

We are switching our course from the M52233DEMO board to the ARM Freedom board.  Is there a convenient way to interface our Project boards, PBMCUSLK, with the Freedom or do we start the interfacing from scratch?

Thanks

Dave Haas

NJIT

Labels (1)
0 Kudos
Reply
1 Reply

1,168 Views
admin
Specialist II

Not directly via the MCU_PORT.  The Freescale Freedom boards outmost row follows the Arduino pin scheme which I am not sure if you can plug that into the breadboard surface.  I don't have the single row of pins to test it out.  (Double rows obviously would not work because you would be shorting two pins together.)

Are you using the NI-ELVIS board in combination with the PBMCUSLK?

~John

0 Kudos
Reply