How do I use the Camera by FRDM-KL25Z?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use the Camera by FRDM-KL25Z?

5,811 Views
yonggunlee
Contributor II

Hello

I am trying to use the camera with FRDM-KL25Z.

What I want to do is line tracking with my robot in the future whenever I finish to build up my robot.

How should I program it in codewarrior to use camera??

Can I only test camera by oscilloscope and see the signal? or is there any interface program that I check the camera is working?

ov7670 camera <-- this is the camera that I want to use with FRDM-KL25Z.

Thank you

0 Kudos
Reply
2 Replies

3,796 Views
FlavioStiffan
NXP Employee
NXP Employee

Use the instructions on the Freescale Cup Knowledge Page for the camera Line Scan Camera Use

0 Kudos
Reply

3,796 Views
yonggunlee
Contributor II

Hello

I checked it, but it was about codewarrior without process expert or component library.

They set it up manually.

Do you know any reference how I can use process expert for camera?

So far, i have set up two different PWM signals, and I was able to see it recognized objects.

But when I use ADC components in component library, i don't know how I should use the value.

Do you have any idea?

Thank you for answering.

0 Kudos
Reply