Gst-Fsl plugins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gst-Fsl plugins

2,114 Views
shafi
Contributor II

Hi

I am working on the IMX6Q platform performing gstreamer applications. For some of the use cases the default demux aiurdemux is not working properly. Could any one give a detailed procedure on how to cross compile gstreamer fsl plugins to be used in the platform. This is required so that I could use the plugins working in PC available in the IMX platform also.Please also share the link where I can find the additional gst-fsl  plugins.

0 Kudos
Reply
1 Reply

1,795 Views
FlavioStiffan
NXP Employee
NXP Employee

I strongly recommend you connect with the i.MX community at i.MX Community and put this question up with the format described in the introduction page. Freescale specialist support the community and will be able to help you

0 Kudos
Reply