大学项目知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

University Programs Knowledge Base

标签

讨论

排序依据:
Welcome to the NXP Cup!  The following pages are designed to introduce students to the concepts of robotics and the components of the NXP Cup Car. Programming microcontrollers is challenging, and the content here is developed to facilitate the process of becoming a successful embedded programmer. General Information Marketplace Special offers from our Global Sponsors History of the NXP Cup Where to buy a racetrack? Mathworks Support for The NXP Cup Race Track Information Community created accessories FAQ's Assembly Directions Keil Software Offer Rules Cameras Regulations Teams' Technical Reports Hardware Concepts Embedded Systems Concepts Real world usage (Practical) Line Scan Camera MCU 101 Tutorials Kinetis FRDM-KL25Z Servo Motor NXP Cup related video series by Prof. Eli Hughes https://community.nxp.com/docs/DOC-1096 Drive (DC) Motors MathWorks basic model for using wide angle lenses on The NXP Cup Car The NXP Cup Technical Reports https://community.nxp.com/docs/DOC-1283 Motor Driver (H-Bridge) https://community.nxp.com/docs/DOC-1057 Battery New Supply location for NXP Cup kits and replacement parts with global delivery possibilities: www.landzo.com CCD sensor: http://www.landzo.com/?product-52.html CCD camera: http://www.landzo.com/?product-51.html Power Motor control unit: http://www.landzo.com/?product-50.html Car kit without Electronics: http://www.landzo.com/?product-49.html In case of any questions or issues, please contact Bella at 汪瑞 <wangrui@landzo.cn> Connect with teams in your region! Brazil EMEA Malaysia Mexico North America Taiwan
查看全文
How does a DC Motor work? The DC motor is a machine that transforms electric energy into mechanical energy in form of rotation. Its movement is produced by the physical behavior of electromagnetism. DC motors have inductors inside, which produce the magnetic field used to generate movement. But how does this magnetic field changes if DC current is being used? An electromagnet, which is a piece of iron wrapped with a wire coil that has voltage applied in its terminals. If two fixed magnets are added in both sides of this electromagnet, the repulsive and attractive forces will produce a torque. Then, there are two problems to solve: feeding the current to the rotating electromagnet without the wires getting twisted, and changing the direction of the current at the appropriate time. Both of these problems are solved using two devices: a split-ring commutator, and a pair of brushes. As it can be seen, the commutator has two segments which are connected to each terminal of the electromagnet, besides the two arrows are the brushes which apply electric current to the rotary electromagnet. In real DC motors it can be found three slots instead of two and two brushes. This way, as the electromagnet is moving its polarity is changing and the shaft may keep rotating. Even if it is simple and sounds that it will work great there are some issues which make these motors energy inefficient and mechanically unstable, the principal problem is due to the timing between each polarity inversion. Since polarity in the electromagnet is changed mechanically, at some velocities polarity is changing too soon, which result in reverse impulses and sometimes in changing too late, generating instantaneous “stops” in rotation. Whatever the case, these issues produce current peaks and mechanical instability. How a DC motor can be controlled? DC motors have only two terminals. If you apply a voltage to these terminals the motor will run, if you invert the terminals position the motor will change its direction. If the motor is running and you suddenly disconnect both terminals the motor will keep rotating but slowing down until stopping. Finally if the motor is running and you suddenly short-circuit both terminals the motor will stop. So there is not a third wire to control a DC motor, but knowing the previous behaviors it can be designed a way to control it, and the solution is an H-bridge. Look at the last evolution of the DC Motor above, you can observe that there are four gates and a motor connected between them. This is the simplest H-bridge, where the four gates represent for transistors. By manipulating these gates and connecting the upper and lower terminals to a voltage supply, you can control the motor in all the behaviors as below. Things to Consider When Using Motors With the Motor and Line scan Camera hooked up to the same board there is a significant problem with noise. The higher you turn the PWM on your drive motors the noise produced and the worse the data will appear from the camera. TO significantly reduce this noise you can simply solder an inductor directly across the 2 drive motors. This will allow you to increase the speed of the car without significantly affecting the data you receive back from the camera.
查看全文
Overview The FRDM-TFC is a convenient "shield" that can drive up to two DC motors (5A per channel), two servos and I/O for the Freescale cup line scan camera and Hall effect sensors.  This board mates with the KL25Z Freedom board for primary usage with a Freescale Cup car. Features: 2 channel Motor Driver ICs (MC33887APVW) 2 channel servo Outputs Dual Linescan Camera interfaces Two inputs for speed sensors Two potentiometers for user functions Two push buttons for user functions 4 Position DIP Switch for user function 4 LEDs (green) for battery indicator or user functions Design Files Rev A is attached to this document. Rev B is attached to this document Code Examples Codewarrior "Bare Metal" Example Code: All Codewarrior based code examples for the FRDM-TFC are hosted on in a Subversion repository on Google Code: frdm-tfc -   Example code for the FRDM-TFC Shield - Google Project Hosting You can check out the code with your favorite SVN client.   Static releases are available in the attachments section of this page.  The current release is "R1.0" mbed.org Example Code: https://mbed.org/components/Freescale-Cup-with-FRDM-KL25Z/ Videos FRDM TFC EXAMPLE CODE GETTING STARTED FRDM-TFC_DEMO 0 and 1 FRDM-TFC_DEMO 2 and 3
查看全文
The line scan camera module consists of a CMOS linear sensor array of 128 pixels and an adjustable lens. This camera has a 1x128 resolution. Line Scan Camera Board Details Schematics, BOM, and datasheets: Line Scan Camera featuring TAOS 1401 Mounting Options You will likely want to mount the camera on a mast or boom above the car to ensure the greatest field of view. Determining the angle of orientation about the pivot at the top of the boom will change the “look ahead” distance of the camera and enable more efficient steering algorithms DIY Camera Mounts Solution Overview One method of implementation is to take the entire readout of the camera and store it in the memory. Then a line detection algorithm can be used to locate the position of the black line. Due to varying lighting conditions, some level of pixel thresholding may be necessary as the intensity differences across the data may not always produce a clear indication of the line location. A good approach is to use an algorithm that looks for changes in the magnitude of voltage from one portion of the array to another, since the camera’s AO magnitude is directly related to the brightness the pixel array senses. If the microcontroller finds a significant decrease in magnitude followed by large increase in magnitude this would give us a good indication of the location of the line. For this a derivative function can be utilized. Once we have successfully determined the position of the black line, immediately adjust the wheels to adjust the direction of the car so that the black line will remain in the center of the camera’s view. Sample camera output (for illustrative purposes only) The camera outputs an analog signal from 0 to 5V depending on the grey-scale value of the image. to simplify our sample we will assume that we have set limits for the line and have transformed the data to digital bits using a threshold value. 0’s are high intensity (non-line locations), 1’s are low intensity (black or line locations) 10000000000000000000000000000000001111101000000000000000000010000000000000000 Since the camera provides a 128x1 bit picture, and the camera will be pointing down at the track which is a fixed width. A control algorithm should be developed to line up the 1’s in the center of the 128 bits. The center of the field of view will be require calibration and testing, but it is assumed that the camera will remain in a fixed location pointing down the center of the forward looking axis of rotation. Signals For normal operation of the camera, the following signals must be produced and processed: CK (clock) - latches SI and clocks pixels out (low to high) continuous signal SI (serial input to sensor) begins a scan / exposure discrete pulses, pulse must go low before rising edge of next clock pulse AO (analog output) - Analog pixel input from the sensor (0-Vdd) or or tri-stated The CK and SI signals are simple ON/OFF signals which can be produce using a GPIO Pin, setting the pin high and low corresponding to the desired exposure time of the camera. The only other requirement is to read the Analog Output of the camera which requires the initialization of the Analog Module and setting it to the proper pinout. Acutal camera output image: Yellow = SI, Green = Camera Signal, Purple = clock More camera waveforms and information (Power Point) available here This link shows a video of the camera connected to the oscilloscope http://www.youtube.com/watch?v=YOAd3ERnXiQ To obtain this signal, connect channel 1, 2 and 3 of an oscilloscope to the SI pulse (Trigger off this signal), CLK, and AO signals. Timing The timing for creation and read of the signals is crucial and is detailed in the diagram below. This information can also be found in the Line Scan Datasheet. Analog Read: The Analog Output (AO) signal from the camera needs to be processed and read by the microcontroller's Analog to Digital Converter (ADC). This ADC device converts a continuous signal into a discrete number which is proportional to the signal voltage. An 8 bit ADC has 256 discrete levels (2^8). If a analog signal between 0 and 5 volts is sampled, a digital discrete number of 0 would correspond to zero volts, and a digital discrete number of 255 would correspond to 5 volts. A number such as 145w would correspond to about 2.8 volts. The maximum signal sample rate is limited by the microcontroller. Proper configuration of the ADC peripheral and the multiplexer of the chip will configure a pin to read in an analog signal when calling the function. More details on analog to digital converters can be found on the wikipedia site here. Read/Write In write mode, the GPIO pin can be set, cleared, or toggled via software initiated register settings. Microcontroller Reference Manual: Analog to Digital Converter You will find high level information about GPIO usage in several different areas of a reference manual. See the reference-manual article for more general information. Relevant Chapters: (see GPIO chapters for clock and SI Creation) Introduction: System Modules: System Integration Modules (SIM) - provides system control and chip configuration registers Chip Configuration: Signal Multiplexing: Port control and interrupts Focusing the camera: Once the sensor is perfectly working the next step is to find the best position of the lens that will generate the clearest images. The best way to do it is using an oscilloscope: Connect the SI and AO signals to the oscilloscope Set the SI pulse so that it can be clearly seen and then trig the AO signal with the SI signal using the trig function Fix the camera looking at a sheet of paper with a black line in the center The image of the black line will appear on the oscilloscope screen Screw the camera until you find the position where the line seems the clearest Camera Circuit   5 wires must be connected ground power SI CLK AO Camera Limitations   According to the datasheet:   " The sensor consists of 128 photodiodes arranged in a linear array. Light energy impinging on a photodiode generates photocurrent, which is integrated by the active integration circuitry associated with that pixel. During the intergration period, a sampling capacitor connects to the output of the integrator through an analog swith. The amount of charge accumulated at each pixel is directly proportional to the light intensity and the integration time." Integration Time: T T = (1/fmax)*(n-18)pixels + 20us, where n is the number of pixels Minimum integration time: 33.75us Maximum integration time: capacitors will saturate if exceeding 100ms frequency range 5 Khz - 8 Mhz (8 Mhz is fmax in equation above) The integration time is the following: It occurs between the 19th CLK cycle and the next SI pulse. The CLK frequency itself has little to do with the integration time. One each rising edge, the clock outputs one of the previously sampled intensity values. This means that integration time should be set by varying the time between SI pulses, not changing the clock frequency. Make the CLK frequency high, and have as much time as needed between the two SI pulses to obtain the desired intensity value. Pro Tips: #1 - Avoid Light Noise Light can be transmitted through the pcb on the back of the camera. This unwanted extra light shining on the CMOS linear sensor can induce significant errors into your signals received. A shroud or housing for the camera unit can easily eliminate this problem. One of the easiest solutions is to place a piece of electrical tape across the back of the camera in the highlighted area indicated in the picture below. #2 - Know your Settings When testing the car on the track or transporting it, it is not uncommon for the focus on the camera to loosen or change. Therefore it is recommended that after adjusting your camera focus for maximum performance you make mark (ex. metallic sharpie) between the lens and its body so you can realign the camera lens to it's proper position easily if it does shift. #3 - Know your Zone When hooking up the linescan camera, regardless of position or focus there is a drop off at each end of the image data. This is easily viewed with an oscilloscope. This effect is undesirable, particularly when you are finding your line position utilizing a derivative approach. These fallouts cause erroneous derivative values, and hence a poor line position solution. Two solutions we found useful were: (1) Ignoring the first 10-15 pixels and last 10-15 pixels of the image data array, and then determining the line position; (2) Often when making decisions in the code as to where the line was at it was found useful to use a threshold value for the difference in the derivative position, and secondly a binary threshold on the camera data. Note that the falloff depends on camera focus, position, etc. Therefore, these threshold values and pixels in which to ignore are relative to a specific instance. The problem however is common to the camera. #4 - Buffer Data Since the camera can read the line very quickly while the servo can only update every 20ms, there are multiple camera reads before the servo can update, if you are reading the camera fast and then overriding without saving them in some form then those camera reads are being wasted and are better off not having occurred. What can help is to create some sort of filter by bringing new values into an array with previous values and preforming some sort of averaging. The following code will take the new line position value and place it in a 1xA array where A is defined by CAMERA_AVG. NO AVERAGING IS OCCURRING HERE all that is happening is the camera values are being saved in a simple array, what is done with them is up to you. The way this works is that it shifts the entire array so the oldest data point is discarded in order to make room for the new line position at the other end of the array. It will only adds the new value if there is one available if not it copies the previous first position value to the new first position value. CAMERA_AVG => an integer value for how long the averaging length will occur gfpLineAverage => global floating point array of camera center line values fpLinePos => returned from read camera this is the center line position ReadCamera() => is the read camera function call returns a floating point value of fpLinePos // this will shift the values up and throw away the oldest value // then add a new reading for (i=CAMERA_AVG;i>0;i—) { gfpLineAverage[i]=gfpLineAverage[i-1]; } // if no line was detected the previous camera value will be passed on if (fpLinePos=ReadCamera()) { gfpLineAverage[0]= fpLinePos; } For example an array of of center line position values ranging from 0-127 could look like. Initial values [51 50 52 54 58 55] New position of 45 read [45 51 50 52 54 58] New position of 44 read [44 45 51 50 52 58] No value read [44 44 45 51 50 52] No value read [44 44 44 45 51 50] New position of 50 read [50 44 44 44 45 51] Program Exercise Specifics of how to configure the K40 ADC, to create the delay code is covered in the K40: Line Scan Camera Tutorial. Additional Training Resources Freescale Motor Control Tutorial Freescale Lecture 1: Introduction and Motor Basics Freescale Lecture 2: Pulse Width Modulaiton Freescale Lecture 3: Control Design Freesacle Lecture 4: Speed and Position Freescale Lecture 5: MPC5607B Overview Additional Resources Freescale app note on interfacing with a linescan camera Freescale app note on interfacing with an RCA camera
查看全文
All results of the NXP CUP survey can be found here.
查看全文
1. Download CodeWarrior 10 Evaluation Version (Eclipse, Windows-hosted) To Program your microcontroller you will need to set up the CodeWarrior Integrated Development Environment. CodeWarrior is available on the Freescale.com Website. Method 1: Direct Link direct download link (Caution - link may not be up to date) Method 2: Navigate to the Download Link From Freescale.com click on: "Design Resources" tab at the top of the page, then navigate to "Software and Tools", and then to "Codewarrior Devleopment Tools" Click on the "Download CodeWarrior now link" Click on the Download Evaluation Versions link" Within this page, use your browser "find" feature (Typically CTRL-F) to search for the text string "Kinetis." Click the "download" button next to "Evaluation: CodeWarrior for Microcontrollers(Eclipse, Windows-hosted) version". and save it to your computer. 2. Install CodeWarrior To install CodeWarrior Development Studio for Microcontrollers v10, double-click the installation package and a wizard will guide you through the installation process. Installation Notes: Are you using Windows Vista or Windows 7? 1. The CodeWarrior installer should be run using the ‘Run as administrator’ option. CodeWarrior service packs are installed with the Eclipse Updater. The updater should also be run with this option. To start the Eclipse Updater select ‘Window > Install new software’ in the menu. 2. Eclipse needs read/write access to the installation folder. Make sure the eclipse installation folder has the appropriate permissions for all users. 3. Make sure your project workspace has read and write permissions Evaluation Edition User: If you are installing the Evaluation Edition, the Evaluation license is automatically installed with your product and you do not need to register it. This license allows you to develop projects as Professional Edition within the 30-day evaluation period. After 30 days, the license works as Special Edition license (free permanent, but feature limited) which supports unlimited assembly code, up to 32KB of C code for HCS08/RS08 derivatives, up to 64KB of C code for V1 ColdFire derivatives and up to 128KB of C code for V2-V4 ColdFire and Kinetis derivatives and up to 512KB of C code for MPC56xx derivatives. Once you have finished downloading and installing CodeWarrior, users can return to Downloading and Installing P&E as part of the Blink a LED on Kinetis Tutorial Additional Resources: CW10 User Manual —The Above user manual has a list of other helpful docs which can be found within your CodeWarrior installation directory. (i.e. <CWInstallDir>\MCU\Help\PDF\)
查看全文
Assembly Of The Freescale Cup Car Chassis Before you start building your program for your car, It would be better if you can assemble your car chassis first. With your car correctly assembled, you can easily test it with your different programs in the later tutorials. The followings are all the tutorials about car chassis assembly. A step-by-step car chassis assembly manual & hints (pub)  (PDF) Servo and steering assembly directions DIY Board mounting template for the TRK-MPC5604B DIY Board mounting template for the Tower System Board mounting suggestions for the FRDM-KL25Z with shield DIY Camera Mounts Wiring connections for the TRK-MPC5604B Hints and notes to chassis assembly Freescale Cup Innovation Challenge EMEA Model B car assembly file in attachment below Exploded Assembly Diagrams Chassis Build Directions [PPT] Original Manufacturer Directions [PDF]
查看全文
The Freescale linescan camera is based upon the TSL1401CL sensor from TAOS Inc. Design Files Schematic & 3D Render (Courtesy of eli_hughes) Images (Lens removed) Freescale Linescan Camera Specifications 128-pixel linear image sensor (TSL1401CL) Focusable imaging lens 5-pin physical interface on PCB on .100" grid Simple three-pin MCU interface with analog pixel output Lens: 7.9mm focal length, f2.4 fixed aperture, manual focus, 12mm x 0.5mm thread Exposure Time: 267µS to 68mS Resolution: 128 pixels Built-In amplifier stage to improve white/black differentiation. The lense used on the board: Alaud Optical     8.0mm f.l. Lens w/IR filter = Part Num: AB0825C        M12x.05 Lens Holder = #9 or #10 Useful links AMS TSL1401 Product Page Line Scan Camera Use Freescale App Note: Line Scan Camera
查看全文
Take some time to get yourself familiar with C programming before you continue on the programming tutorial. Here is a list of topics that you should be comfortable with, and a couple of good tutorials below. Topics included: Program Structure Commenting Variables Keywords Data Types Decimal, Binary and Hexadecimal Equivalents ASCII Text/Number Conversion Math Operators Increment & Decrement Shift Logical Operators Bitwise Operators Loops If Statement Switch Statement Functions Recursion Local Variables vs. Global Arrays Pointers Typdef, struct and union Preprocessor Directives Static, const and Volatile Keywords Tutorial 1: PSU Intro to C for Embedded Design   From PSU Freescale Cup Senior Design Course Tutorial 2: Learning Programming with C This Freescale course consists of a collection of lessons that will introduce you to the fundamentals of programming using the C programming language. Coding for Readability Sometimes when a project has the ability to grow with new features, it is best to code in modules. This allows one to easily take a more modular approach to designing their program. Despite the fact that C does not support Classes like C++ does, you can create structures that can be addressed globally with little code, which is especially useful for microcontroller based projects. An example of a structure which will be made global: This goes in the globals.h file typedef struct {   unsigned char ServoPWM;   char ServoAngle;   unsigned char DrivePWM;   int TimeOut;   int Current;   int Speed; } sMotor; extern volatile sMotor Motor; This will go in any other file that we want our structure to be accessible from #include <Globals.h> volatile sMotor Motor; This is how to address the variable in the structure #include <Globals.h> volatile sMotor Motor; If you decided to have two distinguishable motors you could do this in the globals.h extern volatile sMotor Motor1; extern volatile sMotor Motor2; Then do this in the other files volatile sMotor Motor1; volatile sMotor Motor2; Helpful Hints In developing an algorithm to detect the line position, we found two basic errors in the coding practice which caused catastrophic errors in line detection. Both of these tips are very basic coding practice. First, when using C code, it usually benefits the user to initialize all variables to some value, especially if computations are involved. Often times when the value wasn't initialized it would seem to acquire a wrong value seemingly from nowhere. Secondly, when doing calculations with arrays, make sure to do calculations with array indices that actually exist. Many times we would make the mistake in our loops of trying to use an index that wasn't assigned a value. Therefore it would acquire an unknown value from memory that caused errors in our calculations.
查看全文
Getting Started with the NXP CUP These pages help you with the question of how to achieve the goal of creating an autonomous vehicle that quickly navigates around a track (timed race) and solves precision tasks (Figure 8, Speed limit zone, Obstacle avoidance) What is a Microcontroller? For information on what a microcontroller is head to the microcontrollers article. Getting Started - Learn to Program a microcontroller First off, you are going to need to know C programming. For a crash-course head to c-programming-for-embedded-systems. The classic first application to learn how to program a microcontroller is to get through the process of Blinking an LED. This wiki contains a tutorial for each of the Cup microprocessors which simplifies the process of setting up the evaluation board, installing the Integrated Development Environment, and programming the board with a simple set of software which blinks a LED. The Blink a LED tutorial is the first of 4 tutorials designed to familiarize students with the process of designing a cup car. These four tutorials will introduce students to many of the fundamentals of robotics, the software used to control the locomotion and sensors on an autonomous line following vehicle, and provide example code which help simplify the process of creating a competitive entry in the NXP CUP. Here is an outline of the Basic Microcontroller Programming Tutorial: Read the microcontroller article Choose a microcontroller Set up the development environment Set up the microcontroller evaluation board Program A LED move to the next tutorial… Course Material from the NXP CUP professors and supporters: Thanks to our professors and NXP CUP supporters we created an exclusive starter kit. It includes lecture material, information on the car, useful tips on the board etc. Download the file below and dive into a huge support portfolio! ARC Ingenierie Files - The Champions Board! ARC Ingenierie has been very generous in providing us with their PCB layout and Gerber files to produce your own NXP CUP board. They also provided sample code and drivers plus instructions (in French) to get you started. How cool is that?! Many thanks to ARC, this is much appreciated! Download the files below. If you want to build your own board, please contact us. When do so please keep in mind to give credit to ARC university. All boards should have "HE-ARC Ingenierie" inscription.   Further support links: Information on Line Scan Camera Use The Book of Eli - Microcontrollers, robotics and warp drives Microcontrollers MCU 101 - C Programming for Embedded Systems NXP CUP Shield for the FRDM KL25Z
查看全文
For details on how to use the Motors, visit theDC Motor Tutorial Images Boards before 2013 Current Board Rev. 0 Rev. 1 Technical Details Revision 1 (Schematics, design files, sample code, instructional videos) Revision 0 (Schematics) H-Bridge Specifications Freescale MC33931 Datasheet Pro Tips: #1 - Electro-Magnetic Interfence (EMI) This has been mitigated in the rev. 1 board. In many cases the dc drive motors give off much EM interference causing poor data from the camera, and decreasing the servo motor performance substantially. In most cases around a PWM value of 20-25 duty cycle at the drive motors, caused detrimental problems. This problem was remedied in two ways, (1) connecting capacitors between the motor leads, the closer to the drive motor the better; (2) There is a way to connect the camera directly to the kwikstik and bypass the motor board. #2 - Rev. 0 Board workaround to Enable Braking This has been fixed in the rev. 1 board. In order to go forward AND backwards, you have to have control over IN1 and IN2 (see table below). If you look at the schematic, you can see that IN1 is directly connected to GND. In order to enable breaking you need to lift pin 43, solder a wire to it and control it properly. Tutorials General Tutorial on the DC Motor Control Qorivva: DC Motor Tutorial Kinetis Tower: DC Motor Tutorial Design evolution of motor board prior to 2010 - Freescale Cup Cars utilized the MC33932EVB 2010~2012 - Freescale Cup teams migrated to the current Interface/Motor board featuring Dual H-Bridges [Not manufactured] Tower and Trak Compatible Interface/Motor Control Board (Design files if you want to make one!) 2013+ - FRDM-KL25Z shield
查看全文
Hardware Servos are specialized dc motors geared to produced high-torques and set at specific angles vs rotating continously. The ability to position the servo at a specific angle over and over makes them ideal for robotics, radio controlled car and other various applications. A typical servo will have range of motion from 180-270 degrees. Most modern servos have a three wire interface, red (V+), black (ground), and white (control). To control a servo you must send it a variable length commands (pulse) in 20ms increments. This type of control is called Pulse Width Modulation. Pulse Width Modulation is a square wave with a set period. By changing the width controlling the proportion of on versus off time, you can obtain a digital ratio from 0-100%. That ratio of on versus off time is called the duty cycle. A microcontroller generates a PWM signal using a timer. The time from the beginning of one sequence to the next is called the period. The main timer registers include: Counter, Modulo, Count Initialization Value, Channel Value, FTM Status & Control, and Channel Status & Control. The Counter will count up from the Count Initialization Value and reset after reaching Modulo. One tradeoff of the design is the Modulo value we set. It represents the count value of a full duty cycle and also the resolution of our servo control. Setting a higher Modulo value allows for more precise variation in the servo, i.e. more accurate steering. The downside is that a higher value requires more time per cycle. It is necessary to configure a timer module for the drive motor separate from the servo because they each require different clock frequencies. Another tradeoff of pulse width modulation is whether it is edge-aligned or center-aligned. Edge-aligned PWM, where the channel is cleared at counter overflow and set at channel match, is simpler to implement in hardware. Center-aligned PWM, where the counter counts up and down, is more difficult to implement but does not give as much noise interference when the channel matches. Servos have 3 wires coming out of them: Ground: Black, Brown Power: Red PWM Signal: White, Yellow, Orange Spec Sheet for Servo used in Freescale Cup Futaba-S-3010 Creating the PWM Signal Much of what is needed to create this signal is discussed in the Motor Control tutorial. Click here to review how to configure a PWM signal on your microcontroller. The same microcontroller configuration utilized to drive a motor can be modified slightly to rotate the arm of a servo. Since the Servo and motor require different clock frequencies, it is necessary to configure a timer module for the servo separate from the motor. Freescale Cup participants will configure the timer modules to output signals that control a steering Servo via varying the Duty Cycle of a PWM signal. Microcontroller Reference Manual: Timer Information You will find high level information about Timer usage in several different areas of a reference manual. See the reference-manual article for more general information. Relevant Chapters: Introduction: Timer modules - lists the memory map and register definitions for the GPIO System Modules: System Integration Modules (SIM) - provides system control and chip configuration registers Chip Configuration: Timers Signal Multiplexing: Port control and interrupts Methods of controlling steering angles Construct a look-up table One way of controlling the steering angles is to construct a look-up table. The input of the look-up table can be the shift distance(in pixels) from the center, and the output could be the steering angles. The look-up table can be put into an excel file. So when you want to use it, just copy and paste the table into your code file. Here is an example of how to construct a look-up table. 1. Set up basic parameters of your car: height of camera(h), angle of camera(theta), velocity of car(v), servo delay(s).. 2. Draw a graph to help you develop a function between your input parameters and your output steering angles 3. Put all paraments into excel. So if you want to change any parameters in the future it will be very convenient. 4. Copy and paste look-up table into code file Note: depending on how you define your parameters, the look-up table may not work as well as you expected. Experiments show that the look-up table works well when the shift distance is small( small turns) and the car tends to go off track when the shift distance is big(sharp turns). Poportional Control (P Control) You can map your servo angle based directly on your line location. Take the derivative of the camera signal and use the derivative peaks as the edges of the line. Take the location of each peak and subtract them from each other to get the line width. Taking the min line peak plus line width will give you the location of the line. Now take that location and map it to your servo. We made Camera.Lock = loc and using this we made Motor.ServoAngle = Camera.Lock»1; This made our line location map directly to our servo and it seemed to work well for us. Additional Theory Training Resources Freescale Motor Control Tutorial Freescale Lecture 1: Introduction and Motor Basics Freescale Lecture 2: Pulse Width Modulaiton Freescale Lecture 3: Control Design Freesacle Lecture 4: Speed and Position Freescale Lecture 5: MPC5607B Overview
查看全文
Overview This document has links to videos to give tutorials on how to getting started *from scratch* with the freedom board.    In these tutorials we build projects with bare metal code to see how things work!   It includes the basics on how to get clocks running,  lights blinking and interrupts firing *from scratch*. For more code/peripheral examples that use a "bare metal" approach,  check out the page on the FRDM-TFC board. ERRATA!!!   While working with a large number of Freedom boards in a course,  it was observed that the InitClockRoutines would *sometimes* not work.    *Some* of the crystals on the freedom boards do NOT like "HIGH_GAIN" mode.   The new code is uploaded to this page but you could also change the code yourself:   pll_init(8000000, HIGH_GAIN, CRYSTAL, 4, 24, MCGOUT); to   pll_init(8000000, LOW_POWER, CRYSTAL, 4, 24, MCGOUT); Projects From Scratch for the Freedom Board with Codewarrior 10.3 Projects From Scratch - Part 2 - Importing other projects Using the Freescale Header Files and Blinking the LED Source code for video (Codewarrior 10.3) is in the attached files at the bottom of this document. Clock Distribution Source Code for the Clock Distribution video is in the attached files at the bottom of this document. Interrupts Part 1 - Background Interrupts Part 2 - ARM Systick Timer Source Code for the ARM Systick Timer video is in the attached files at the bottom of this document. Interrupts Part 3 - TPM (Timer Pulse Width Modulator) Overflow Source Code for the TPM Overflow Interrupts video is in the attached files at the bottom of this document
查看全文
Further Reading MCU 101: How does a DC Motor work? MCU 101: Pulse Width Modulation for DC Motors Specifications of Included DC Motor Conditions of Standard Operation Driving Voltage: 7.2V Direction of Rotation: CW viewing from metal housing Position of Motor: Horizontal Operating Temperature: 10 to 30 (Celsius) Operating Humidity: 30%RH to 95%RH Electrical Characteristics No Load Speed: 16000+/- 3200 rpm No Load Current 220mA (max) Mechanical Noise (Distance from housing side A=10cm Background Noise =30dB (max) 75 dB Stall Current: (two points method 1.2&3.9mNm) 3800mA (max) Stall Torque (two points method 1.2&3.9mNm) 80g.cm min End Play of Shaft 0.05~0.60 mm
查看全文
Some typical variations: Report Requirements Specific Components Usage Additional Tiers of Competition 2017 Rules per Region EMEA University Challenge 2016-2017 2016 Rules per Region Americas, Malaysia and Taiwan.​ EMEA University Program Challenge EMEA High School Challenge 2015 Rules per Region Worldwide Challenge Rules EMEA 2014 Rules per Region EMEA Worldwide Challenge Rules USA [ARCHIVE] 2013 Rules per Region Malaysia Latin America Latin America - Advanced USA Global Championship
查看全文
1. Overview 2. Hardware 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup 4. Build the Code 5. Download/Debug/Run 6.Example Code Functions ImageCapture(); ReadADCChannel() Initialize the ADC Header File Definitions Initialize the GPIO Other Tutorials: This tutorial covers the details of obtaining data from the line scan camera on the Kinetis K40 using the TWR-K40X256-KIT evaluation board. General details of the line scan camera not related to the Kinetis can be found in the general Line Scan Camera Theory article. This tutorial will help students familiarize themselves with how to interface the camera with the microcontroller, how to configure GPIO pins to create clock signals and also how to utilize the microcontroller's ADC to read the data from the camera. Outside of control algorithms, configuring the camera is one of the more complex tasks necessary to create a Freescale Cup Vehicle. 1.  Overview In this exercise students will access the line scan camera, create a clock signal and create the initialization pulse which tells the camera to begin the exposure period. This tutorial will not describe line recognition or line following algorithms - these concepts are beyond its scope. Students will: Create the code using Codewarrior Build a project Download the code to the board connect the microcontroller to the camera. Run the program view the camera data, clock and Si pulse on an oscilloscope view the data from the camera in the CodeWarrior Debugger for verification purposes   To successfully complete this exercise, the following software and hardware are required: The K40 Tower card, TWR-K40x256 CodeWarrior for Microcontrollers Freescale Line Scan Camera Motor Board Tower Prototyping board Soldering Iron Solder Tower Elevators USB Cord 2. Hardware   Read the Line Scan Camera Overview article for general information on the camera, ADC, and GPIO microcontroller configuration settings. 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup It is crucial for an engineer to have the proper test equipment and tools for the job. In this case, without an oscilloscope, students will not be able to verify whether the proper signals are being sent to the camera. 4. Build the Code If there is more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. If errors are encountered, look in the Problems view and resolve them. For now ignore any warnings. 5. Download/Debug/Run Download the code to your board, once this process is complete resume the project so that the code runs. If you want more information on how to complete this step see the download debug run section of the Kinetis Blinking Led tutorial. 6.Example Code What will happen: the function ImageCapture() is called in main.c with a pointer to the first element in the array. This function completes the processes necessary to capture images using the camera. To become more familiar with Pointers and Arrays - navigate to the C Programming Tutorial. Knowledge of Pointers and Arrays is a pre-requisite for understanding the Camera Code. Functions The camera code utilizes the following function: within main.c ImageCapture(&Line.RawCameraData[0]); is called to initiate the step of capturing an image into the first position of the array. ImageCapture(); from Camerainterface.c This function captures the images by creating the SI Pulse, and clock signals, capturing the data into an Array using the ADC features of the K40. It calls the function ReadADCChannel() at the proper time which then inputs data from the camera AO line. void ImageCapture(int * ImageData){//this is a pointer to a single character in memory   unsigned char i;   TAOS_SI_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_SI_LOW;   TAOS_EXPOSURE_DELAY;   ImageData[0] = (int)ReadADCChannel(19);// inputs data from camera (first pixel)   TAOS_CLK_LOW;   for(i=1;i<128;i++)   {   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   ImageData[i] = (int)ReadADCChannel(19); // inputs data from camera (one pixel each time through loop)   TAOS_CLK_LOW;   }   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_HIGH;   TAOS_EXPOSURE_DELAY;   TAOS_EXPOSURE_DELAY;   TAOS_CLK_LOW;  } ReadADCChannel() from readADC.c this function does the analog to digital conversion and returns a value between 0 and 255. It takes the proper ADC channel, in this case 19. Channel 19 corresponds to analog input pin ADC1_DM0 (see page 117 in the K40 Sub-Family Reference Manual). unsigned char ReadADCChannel(unsigned char Channel)   {   ADC1_SC1A = Channel;   while((ADC1_SC1A & ADC_SC1_COCO_MASK) == 0)   {   }   return ADC1_RA;    } Initialize the ADC Before utilizing the ADC it must be calibrated and initialized. The details for how to do this can be found in Chapter 19 Using Peripheral Delay Block (PDB) to Schedule Analog to Digital Converter (ADC) Conversions of the Kinetis Peripheral Module Quick Reference manual. The PDB portions of the code have been removed for the Cup Car Demo Code. Header File Definitions from k40_TOWER_BOARD_SUPPORT.h The following code enables the GPIO on the two pins: #define TAOS_CLK_LOC (1<<28) #define TAOS_SI_LOC (1<<18) Initialize the GPIO From K40_TOWER_BOARD_SUPPORT.c The InitK40GPIO Function sets up the ports for use: Relevant code SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK; //CLK and SI signal PORTC_PCR18 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK; PORTE_PCR28 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK; //Make Sure the GPIO is setup to be an output GPIOC_PDDR |= LED_E1_LOC | LED_E2_LOC | LED_E3_LOC | TAOS_SI_LOC; GPIOE_PDDR |= TAOS_CLK_LOC; GPIOB_PDDR |= LED_E4_LOC; Other Tutorials: K40:Blinking LED Tutorial K40:Drive DC Motor Tutorial K40:Turning a Servo Tutorial   
查看全文
This tutorial covers the details of Blinking an LED on the Kinetis K40 using the TWR-K40X256-KIT evaluation board. It will introduce the evaluation board, and some basic CodeWarrior features. Overview 1. Hardware 2. Set up the Software Development Environment A. Download and Install Codewarrior B. Download and Install Drivers 3. Set up the Hardware: Twr K40x256 Hardware Setup 4. Import the LED Project 5. Build the Code 6. Download/Debug/Run 7. Learning Step: LED Code Description Read/Write Functions Variables Header File Definitions Initialize the GPIO Blink the LED: Other K40 Tutorials: K40 Related Pages Credits / References Overview   In this exercise students will explore a Freescale Cup Car application which targets a Freescale K40 board attached to the Tower System.   Students will: Configure the Software Development Environment Configure the evaluation board hardware Learn how to import example files into a CodeWarrior project Build a project Download and run the code on a Kinetis K40 Tower System board Learn how to utilize the GPIO Peripheral to blink a LED     To successfully complete this exercise, students will need the following board and development environment. The K40 Tower card, TWR-K40x256 CodeWarrior for Microcontrollers USB Cord 1. Hardware     Read the Blink LED overview article for general information on LED circuits, GPIO pins and reference manuals.   2. Set up the Software Development Environment   There are several steps necessary to prepare the evaluation board and PC for microcontroller programming and development. Interfacing the evaluation board with a PC requires downloading and Install the CodeWarrior IDE, as well as the device drivers for programming the microcontroller via USB. A. Download and Install Codewarrior   Before completing this example project, download-and-install-codewarrior-10-1 or the latest version compatible with the twr-k40x256-kit.   B. Download and Install Drivers   In addition to CodeWarrior, it may(needs verified) be necessary to install one or both of the following tools: RAppID initialization tool- RAppID comes on the DVD provided with your evaluation board. In the main directory of the DVD, click on the "TRK_MPC5604B.html" file to open the DVD interface which provides user manuals, software, schematics and documentation for the evaluation board. P&E Microcomputer Systems, Inc drivers- P&E is a a computer driver for the TRK-MPC5604B and Kinetis Tower system device, enabling evaluation board programming via USB through the CodeWarrior debug OSJTAG interface. This driver can be downloaded here in case this isn't found on the disk.   3. Set up the Hardware: Twr K40x256 Hardware Setup   There are several Twr K40x256 hardware configuration steps. Follow the twr-k40x256-hardware-setup instructions before importing the LED Project. 4. Import the LED Project   After the software is successfully downloaded and installed, the next step is to import an existing project into your Workspace. in this case, the LED_BLINK_96MHZ Project. Follow the instructions on the codewarrior-project-import page to import the LED_BLINK_96MHZ project into CodeWarrior. If errors are encountered, look in the Problems view and resolve them. Ignore any warnings. 5. Build the Code   If there is more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. By default, the application is set to link to RAM. If you want your program in FLASH, make sure that you have that build configuration enabled:     Make sure you do a "Clean" operation (under the project menu) after you make the configuration change. If you encounter errors, look in the problems view and resolve them. You can ignore any warnings. 6. Download/Debug/Run   If the project builds correctly, it is time to download to the board and watch it work. Ensure that the USB cable that came with the board connects the board to the host computer’s USB port. There are multiple ways to issue the Debug command. Right click the project in the projects view and choose Debug As->CodeWarrior Download. Alternatively, y go to the Run menu and choose Debug (F11). Click the Resume button and your should see the LED blinking! Click the Pause button to stop execution. Click the Terminate button to end debugging. 7. Learning Step: LED Code Description Read/Write   If the LED was on Port C, Bit 7 we might have code like: #define LED_E1_Location(1<<7)   For example, to toggle a pin the following code might be used: GPIOC_PSOR=LED_E1_LOC     "Sets" the LED located at "E1" high.   the syntax means the following GPIOC refers to Port C   "Set" is one of three commonly utilized commands for GPIO control. There are also commands for "Clear" and "Toggle."   Command: "GPIOC_PSOR" literally means PORT SET OUTPUT REGISTER which SETS a pin high Command: "GPIOC_PCOR" clears a pin, PORT CLEAR OUTPUT REGISTER which CLEARS a pin to the "low" state Command: "GPIOC_PTOR" toggles a pin opposite of the current state   the « is a "shift" command which is discussed in the c-programming-for-embedded-systems. You can alter the raw register as well using a MASK but the dedicated set/clear/toggle registers are more straightforward.   **NEEDS UPDATED ** Hardware Chip Port/Pin Comment SW3 PT cell-content SW4 cell-content cell-content Functions   The following functions can access the LED; //Where n is the LED number LED_En_TOGGLE;  //will toggle a LED to a different state LED_En_ON; // turns the LED ON LED_En_OFF // turns the LED OFF Variables   Locations of the LED's LED_E1_LOC LED_E2_LOC LED_E3_LOC LED_E4_LOC Header File Definitions   from k40_TOWER_BOARD_SUPPORT.h //The E1 LED is on Port C, Bit 7 #define LED_E1_LOC (1<<7) #define LED_E2_LOC (1<<8) #define LED_E3_LOC (1<<9) #define LED_E4_LOC (1<<11)    //There are dedicated set and clear registers.    //Write a one to PSOR Sets the Bits, Writing to PCOR clears bits.    //Toggling a bit can be done with the PTOR register    //You can access the raw register as well -> PDOR |= My Bit    //but the dedicated bit set/clear/toggle registers are easier!    //Also, The cathode of the LEDs are towards the port pin! This means    //you have to turn the port off to get the LED to turn the pin on. #define LED_E1_OFF   GPIOC_PSOR=LED_E1_LOC #define LED_E1_ON   GPIOC_PCOR=LED_E1_LOC #define LED_E1_TOGGLE   GPIOC_PTOR=LED_E1_LOC #define LED_E2_OFF   GPIOC_PSOR=LED_E2_LOC #define LED_E2_ON   GPIOC_PCOR=LED_E2_LOC #define LED_E2_TOGGLE   GPIOC_PTOR=LED_E2_LOC #define LED_E3_OFF   GPIOC_PSOR=LED_E3_LOC #define LED_E3_ON   GPIOC_PCOR=LED_E3_LOC #define LED_E3_TOGGLE   GPIOC_PTOR=LED_E3_LOC #define LED_E4_OFF   GPIOB_PSOR=LED_E4_LOC #define LED_E4_ON   GPIOB_PCOR=LED_E4_LOC #define LED_E4_TOGGLE   GPIOB_PTOR=LED_E4_LOC Initialize the GPIO   From K40_TOWER_BOARD_SUPPORT.c void InitK40GPIO() {    SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;    //To use a Port, its Clock must be enabled!!    //Lets just enable the clocks for ALL of the ports    //Important! Each IO pin has a dedicated 32-bit Register to set it up (Selection GPIO vs peripheral, IRQ, Etc.)    //Setup port C7,C8,C9 and B11 as GPIO and enable High Drive Strength    PORTC_PCR7 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;  //Enable GPIO on on the pin    PORTC_PCR8 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;  //Enable GPIO on on the pin    PORTC_PCR9 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;  //Enable GPIO on on the pin    PORTB_PCR11 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;  //Enable GPIO on on the pin    PORTC_PCR18 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;    PORTE_PCR28 = PORT_PCR_MUX(1) | PORT_PCR_DSE_MASK;    //Make Sure the GPIO is setup to be an output    GPIOC_PDDR |= LED_E1_LOC | LED_E2_LOC | LED_E3_LOC;    GPIOB_PDDR |= LED_E4_LOC;    LED_E1_OFF;    LED_E2_OFF;    LED_E3_OFF;    LED_E4_OFF; } Blink the LED:   Within Main.c or any other C file created, Blink the LED's using the following functions: LED_E1_TOGGLE; LED_E1_ON; LED_E2_OFF; Other K40 Tutorials:   K40 Related Pages   K40: Turning A Servo Tutorial   K40: Drive DC Motor Tutorial Kinetis K40 TWR-K40X256 K40: Blinking LED Credits / References   Some of the content from this tutorial originated from:   Shawn Moffit: Electrical Engineering, Penn State University for - K40 Code   Processor Expert Hands-On Lab Rev. 1.0, 05/2011 by Jim Trudeau, Freescale Semiconductor, Inc. for - some text descriptions of steps Original Attachment has been moved to: LED_BLINK_96MHZ.zip
查看全文
This tutorial covers the specific details of obtaining data from the line scan camera on the Qorivva TRK-MPC5604B board. This tutorial will help students familiarize themselves with how to interface the camera with the microcontroller, how to configure GPIO pins to create clock signals and also how to utilize the microcontroller's ADC to read the data from the camera. Outside of control algorithms, configuring the camera is one of the more complex tasks necessary to create a Freescale Cup Vehicle. 1. Overview 2. Hardware 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup 4. Build the Code 5. Download/Debug/Run 6. Learning Step Functions Calling the Function Variables Setting threshold. (This can give you a simple view of what your camera sees without connecting it to a scope) Sample Code Download Link Alternative Examples Other Qorivva Tutorials: Links External 1. Overview In this exercise students will access the line scan camera, create a clock signal and create the initialization pulse which tells the camera to begin the exposure period. This tutorial will not describe line recognition or line following algorithms - these concepts are beyond its scope. Students will: Open the example file using Codewarrior Build a project Download the code to the board connect the microcontroller to the camera via the motor control board Run the program view the camera data, clock and Si pulse on an oscilloscope To successfully complete this exercise, students will need the following board and development environment: TRK-MPC5604B Motor Drive Board Version A Freescale Cup TRK-MPC5604B compatible Car Kit CodeWarrior for Microcontrollers v 2.8 P&E Micro Toolkit Freescale Line Scan Camera USB Cord Knowledge of how Pointers and arrays are utilized in C 2. Hardware   Read the Obtain Data From Line Scan Camera overview article for general information on the camera, ADC, and GPIO microcontroller configuration settings. Connect the sensors, motor drive board and microcontroller of your car according to the TRK-MPC5604B chassis build instructions 3. Set up the Hardware: Line Scan Camera/Microcontroller Hardware Setup It is crucial for an engineer to have the proper test equipment and tools for the job. In this case, without an oscilloscope, students will not be able to verify whether the proper signals are being sent to the camera, or that the camera is working properly. 4. Build the Code If there is more than one project in your project view, make sure the proper project is the focus. The most reliable way to do this is to right click the project and choose Build Project as shown below. You can also go to the Project menu and choose the same command. If errors are encountered, look in the Problems view and resolve them. For now ignore any warnings. 5. Download/Debug/Run Download the code to your board, once this process is complete resume the project so that the code runs. 6. Learning Step What will happen: the function ImageCapture() is called in main.c with a pointer to the first element in the array. This function completes the processes necessary to capture images using the camera. To become more familiar with Pointers and Arrays - navigate to the C Programming Tutorial. Knowledge of Pointers and Arrays is a pre-requisite for understanding the Camera Code. Functions void CAMERA(void) {   TransmitData("****Line Sensor Test****\n\r");   SIU.PCR[27].R = 0x0200; /* Program the Sensor read start pin as output*/   SIU.PCR[29].R = 0x0200; /* Program the Sensor Clock pin as output*/   for(j=0;j<2;j++)   //for(;;)   {   SIU.PCR[27].R = 0x0200; /* Program the Sensor read start pin as output*/   SIU.PCR[29].R = 0x0200; /* Program the Sensor Clock pin as output*/   SIU.PGPDO[0].R &= ~0x00000014; /* All port line low */   SIU.PGPDO[0].R |= 0x00000010; /* Sensor read start High */   Delay();   SIU.PGPDO[0].R |= 0x00000004; /* Sensor Clock High */   Delay();   SIU.PGPDO[0].R &= ~0x00000010; /* Sensor read start Low */   Delay();   SIU.PGPDO[0].R &= ~0x00000004; /* Sensor Clock Low */   Delay();   for (i=0;i<128;i++)   {   Delay();   SIU.PGPDO[0].R |= 0x00000004; /* Sensor Clock High */   ADC.MCR.B.NSTART=1; /* Trigger normal conversions for ADC0 */   while (ADC.MCR.B.NSTART == 1) {};   adcdata = ADC.CDR[0].B.CDATA;   Delay();   SIU.PGPDO[0].R &= ~0x00000004; /* Sensor Clock Low */   Result[i] = (uint8_t)(adcdata >> 2);    }   Delaycamera();   //printlistall();   }   printlistall(); } Calling the Function within the main for loop in main.c, call the camera function using the following code: for (;;)   {   CAMERA();   } Variables Creates an 128x1 array for camera data information volatile uint8_t Result[128]; /* Read converstion result from ADC input ANS0 */   Setting threshold. (This can give you a simple view of what your camera sees without connecting it to a scope) #define THRESHOLD (2.0 /*volts*/ / 0.03125) // 8-bit A/D = 31.25mV/bit CAMERA(); // read line sensor, 128x1 pixel result returned in Result[128] array // print result for (i = 16; i < 112; ++i) // ignore the first and last 16 bits in the camera frame   if (Result[i] < THRESHOLD)   TransmitCharacter('1'); // black (low intensity)   else   TransmitCharacter('0'); // white (high intensity) Sample Code Download Link Qorivva Sample Code Download Link Alternative Examples Application Note 4244 and Software. Other Qorivva Tutorials: 1. Qorivva: Blink LED 2. Qorivva: Drive DC Motor Tutorial 3. Qorivva: Turning A Servo 4. Qorivva: Line Scan Camera Tutorial Links Qorivva Overview https://community.nxp.com/docs/DOC-1019 External TRK-MPC5064B Freescale Webpage TRK-MPC5064B Freescale Reference Manual TRK-MPC5064B Freescale Schematic
查看全文
All information can be found in this document
查看全文
The Kwikstik board is a great board for use in a Freescale Cup car! This page has some videos and example code to get you up and running quickly. For novice embedded developers it is recommended you use the FRDM-KL25Z for your Freescale Cup car. Board Tips The General Purpose TWRPI socket on the Kwikstik K40 board provides access to I2C, SPI, IRQs, GPIOs, timers, analog conversion signals, TWRPI ID signals, reset, and voltage supplies. The pinout for the TWRPI Socket is defined in Kwikstik User's Manual, but the user manual does not describe how to order a connector. Soldering and directly connecting to the pins on the socket itself is very risky and not recommended. When browsing for connectors that interface with the TWRPI sockets you have two main options. 1. The first is a surface mount chip, that is a female connector to connect with the male pins on the board. There are surface mount lead on the top of the chip which will be easier to solder to. The part number is: SFC-110-T2-L-D-A 2. The second option is a female connector which mates with the male connection on the board and is then terminated with a wire for each pin. This option can greatly simplify your wiring challenges on your car as any additional lengths or wires can easily be trimmed off. The part number is: SFSD-10-28-G-12.00-S Image of the SFSD-10-28-G-12.00-S with corresponding Kwikstik TWRPI socket. Connectors can be ordered from Samtec as samples at this website: [http://www.samtec.com/suddenservice/samples/samples.aspx] Useful Videos:   Creating a new baremetal project for a Freescale KwikStik http://www.youtube.com/watch?v=P8X079Qs7cg&feature=g-upl&context=G2f166b6AUAAAAAAADAA   Debugging a bare metal project on the Freescale Kwikstik. http://www.youtube.com/watch?v=nQhhfNJZL_o&feature=g-upl&context=G2dcfcd5AUAAAAAAAEAA   Importing projects and merging code. http://www.youtube.com/watch?v=A_h9W-QRHp8&feature=g-upl&context=G2354416AUAAAAAAACAA   A discussion of the header files (and how to use them!) for Kinetis Devices in Codewarrior V10. This is the first of 2 videos. I had to split them up as I cannot upload videos greater than 15 minutes in length. http://www.youtube.com/watch?v=EP2FydCX9tY&feature=g-upl&context=G2fdf3fcAUAAAAAAABAA   Second part of the Kinetis Header file discussion http://www.youtube.com/watch?v=ygjx-OkJuS4&feature=g-upl&context=G2792e97AUAAAAAAAAAA   Discussion on getting the Clock setup on the Kwikstik http://www.youtube.com/watch?v=_FQzXhLDP2w&feature=youtu.be   How to setup GPIO on the Kinetis. Includes discussion on enabled clocks to peripherals and setting up the pin control registers. http://www.youtube.com/watch?v=GXjRpsGJJt4&feature=youtu.be   How to use the SysTick peripheral in the Cortex core with interrupts http://youtu.be/8SRqlDkJwGU   Discussion of how to setup interrupts on the NVIC. The Flex timer is used as an example http://www.youtube.com/watch?v=_mClHzxm0Wk&feature=youtu.be   Example Programs: All of the programs are bare metal examples for CodeWarrior 10.1 that can be used on the Kwikstik board. Make sure to read all of the comments in the C files! How to Load Programs In CodeWarrior: Copy only the source files and header files into a new folder. Import that new folder into CodeWarrior to avoid debug problems.   ClockSetup - Systick This example will demonstrates how to enable the 4MHz Crystal on the Kwikstik. Early versions of the Kinetis silicon had bug in which the device could crash if the clock dividers are changed while executing from FLASH (errata e2448). This code places clock initialization code in RAM. The clock code is based upon routines from Kinetis Peripheral Module Quick Reference (Freescale document KQRUG.pdf). It also shows how to enable the SysTick module in the Cortex Core. The SysTick is used to provide a delay Function. ClockSetup - SysTick.zip     FlexTimer_NVIC_IRQ This code shows how to use the NVIC in the Cortex Core. The Flex Timer module is used to generate a periodic interrupt (similar to the SysTick example). FlexTimer_NVIC_IRQ.zip   LCD_Example This code will turn on segments on the LCD on the Kwikstik. The LCD driver code is derived from the MQX based example on the Kwikstik page. LCD_Example.zip   PWM_Test This code shows how to setup the flex timers to generate different styles of PWM. Note: One of the examples sets up the flex timer for pseudo-complementary PWM. It DOES NOT use the hardware based complementary mode. It writes 2 individual registers in a software routine. One should use this a starting point to enable full hardware based complementary mode. PWM_Test.zip   CameraTest This example is a basic example on how to interface to the Freescale Linescan Camera. It will display a rough approximation of the output on the LCD. CameraTest.zip Note: The code does not run with the camera by default. This is because the AOUT is set to the pin with the pull up resistor (J15 pin 4). Once changed it will work smoothly.
查看全文