ユニバーシティ・プログラムのナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

University Programs Knowledge Base

ディスカッション

ソート順:
The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.
記事全体を表示
1. Overview   This module demonstrates how to implement a steering control system using Pulse Width Modulation (PWM) on NXP S32K3 microcontrollers. The application reads an analog input from a potentiometer (simulating a steering wheel) and converts it into a servo motor position. As the input changes, the servo motor reacts in real time, mimicking how steering systems work in modern vehicles. This example is based on Application Code Hub demonstrations for: PWM-Based Steering Control for FRDM-A-S32K344 PWM-Based Steering Control for FRDM-A-S32K312 In this workshop, a POT Click simulates the steering wheel position. When the student rotates it, an analog voltage proportional to the angle is read by the MCU through the ADC, scaled in software, and converted into a PWM duty cycle. The PWM is generated by the Servo Click (configured by the MCU over I²C) and drives a Micro Servo motor SG 180°, whose angle tracks the potentiometer in real time. Beyond the technical implementation, the course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.   2. Learning Scope   After completing this course, participants should be able to:   Understand a basic steering control system and the ideas behind EPS and steer-by-wire. Use the POT Click as a simulated steering-wheel input. Acquire analog values (0–3.3 V) using the ADC and understand analog-to-digital conversion. Perform signal scaling from the ADC range to a servo angle / PWM duty cycle. Generate PWM signals to drive a servo motor. Configure the Servo Click over I²C using the OE (Output Enable) pin. Recognize the actuation data flow: sensor input → MCU processing → PWM actuation. Import, build, flash, and debug an ACH project in S32 Design Studio 3.6.5. Understand why steering functions are relevant for functional safety. 3. System Architecture   The three elements capture exactly the basic idea of the system in the demo: Input: Potentiometer (POT Click simulates the steering-wheel position) Processing: S32K3 MCU (reads the ADC, scales the value, commands the actuator) Output: Servo motor controlled via PWM (Micro Servo SG 180°) This matches the classic flow of an embedded actuation system: sensor → processing → actuator. Functional Flow The system operates continuously as follows: The potentiometer generates an analog voltage based on its position The ADC converts this voltage into a digital value The application scales this value into a steering angle The system generates a PWM signal based on the angle The servo motor moves accordingly This loop runs continuously to ensure real-time control. Steering Monitoring Application Architecture 4. Key Concepts   4.1 ADC (Analog-to-Digital Converter) The POT Click outputs 0–3.3 V depending on the wiper position. The ADC samples this voltage at regular intervals and quantizes it into a digital code (a 12-bit ADC produces values between 0 and 4095). The further the potentiometer is turned, the higher (or lower) the digital sample. ADC acquisition is the foundation of automotive sensing — used for torque, throttle, battery voltage, and many others. 4.2 Signal Scaling — From ADC to Servo Angle The ADC range (for example 0–4095) and the servo range (0°–180°, expressed as a PWM duty cycle) are different. The application performs a linear mapping so that one end of the potentiometer corresponds to one steering extreme and the other end to the opposite. This is the same scaling used in real EPS systems, where a hardware reading is converted into a normalized control command. 4.3 PWM — Pulse-Width Modulation and Servo Control PWM switches a digital output on and off at a fixed frequency, varying the duty cycle (the fraction of time the signal is high). A hobby servo such as the SG 180° interprets this duty cycle as a position command. In this demo, the PWM is not generated by the MCU itself but by the Servo Click's dedicated PWM controller, which the MCU configures over I²C — a typical embedded pattern that offloads time-critical signal generation and keeps the CPU free for application logic. 4.4 I²C — Configuring the Servo Click I²C — Inter-Integrated Circuit is a two-wire serial bus made of SDA (data) and SCL (clock). The S32K3 uses LPI2C1 on PTC6 (SDA) and PTC7 (SCL) to configure the Servo Click — PWM frequency, channel, and duty cycle. The OE — Output Enable pin on PTB17 is an additional control line that enables or disables the PWM outputs without reconfiguring the chip, which is also useful for a quick "safe stop" behavior. 4.5 POT Click as Steering Wheel The POT Click is a simplified, safe stand-in for a real steering sensor. The student rotates it by hand, the voltage changes, the MCU reads it through the ADC, scales it, and the servo reacts. 4.6 Data Flow at a Glance Physical rotation → analog voltage → ADC sample → scaled command (angle / duty cycle) → I²C configuration of the Servo Click → PWM signal → servo angle. This direct chain from the student's hand to the servo shaft is the main educational value of the demo. 5. Hardware and Software Setup   Required Hardware Component Image Purpose FRDM-A-S32K312 Alternative MCU platform used to run the steering application and process steering inputs. FRDM-A-S32K344 Alternative MCU platform used to run the steering application and control connected peripherals. FRDM-K64 Click Shield mikroBUS expansion board used to connect Click modules to the FRDM platform. Servo Click PWM driver board used to control the servo motor position. POT Click   Potentiometer module used to simulate steering wheel input. Micro Servo SG 180°                     Actuator used to convert control signals into steering movement. USB-C / 12 V supply — Provides power and enables programming and debugging of the system.   The example applications demonstrate how these peripherals are connected to the MCU pins and used to simulate steering wheel input and actuator control.   Steering Control Monitoring on FRDM-A-S32K312 Steering Control Monitoring on FRDM-A-S32K344       Software Environment S32 Design Studio IDE S32K3 Automotive Software Package Application Code Hub project import PWM-Based Steering Control for FRDM-A-S32K344 PWM-Based Steering Control for FRDM-A-S32K312 6. Implementation Guide   Step Action Sub-steps Expected Result 1 Import the Project Open S32 Design Studio Select “Import project from Application Code Hub” Search for the steering demo Use the GitHub link for automatic configuration Select main branch Import project Project successfully appears in workspace 2 Build the Application Right-click project Select “Update Code and Build Project” Confirm SDK component management Build completes with no errors and generates .elf file 3 Connect Hardware Connect USB cable (and 12V supply for S32K312) Attach click boards Verify wiring Board is powered and detected by IDE 4 Flash and Run Open Debug Configurations Select “debug_flash_pemicro” Start debugging Application runs continuously 5 Functional Validation Rotate the potentiometer Observe servo movement Servo follows potentiometer position in real time   7. Signal Behavior and Control Logic     Figure: Steering control signal mapping. The 12-bit ADC value (0–4095) is linearly mapped to a servo angle (0°–180°) and a matching PWM duty cycle (1.0–2.0 ms), with reference points at Left, Center and Right. At startup the servo moves to the neutral position; during operation, any input change produces an immediate, proportional reaction — implementing a basic steer-by-wire behavior.   8. Troubleshooting   Issue Possible Actions Board Not Detected Check USB cable and drivers Verify debugger connection Restart IDE No Servo Movement Verify PWM configuration Check servo wiring Ensure correct power supply Incorrect Behavior Check ADC configuration Validate scaling function Ensure PWM duty cycle mapping is correct Unstable Movement Add signal filtering Check power stability   9. Extending the Application   The basic implementation can be extended in several ways: Steering Range Control Restrict or extend the actuator's range of motion Define software-based limits to protect the mechanics Input Direction Inversion Reverse how the actuator responds to the input Useful for left-hand vs. right-hand drive calibration Noise Filtering Apply software filtering to stabilize readings Avoid jitter near the center position Scaling Logic Exploration Identify and analyze how the input is mapped to the output Connect software math with hardware behavior Fault-Handling Behavior Add a mechanism that reacts to a detected fault Transition the system into a safer state State Machine Implementation A more advanced approach is to implement a state machine: Idle Active Fault 10. Safety Context   This example reflects key automotive principles: Continuous monitoring of driver input Immediate response to control signals Reliable actuator control In real systems: Redundancy is required Fault detection mechanisms are implemented Systems must comply with ISO 26262 (functional safety standard) Steer-by-wire systems require high reliability since there is no direct mechanical link. 11. Conclusion   This module demonstrates how a simple embedded system can implement steering control using ADC input and PWM output. It shows how: Analog input is acquired Data is processed in real time Actuators are controlled using PWM   Result on FRDM-A-S32K312 Result on FRDM-A-S32K344   The course provides a strong foundation for more advanced systems, including filtering, state machines, and safety-oriented designs.
記事全体を表示
1. Overview   This article is the umbrella entry point for a series of automotive embedded workshops built on the FRDM-A-S32K3xx microcontroller family. It groups together five hands-on modules — Lights, Brakes, Steering, Comfort, and Transmission — each demonstrating a different real-world automotive function that a modern Body Control Module (BCM), Chassis ECU, or Powertrain ECU would implement in production vehicles. All five modules share the same educational philosophy: they take a simple, low-risk hardware setup (FRDM board + FRDM-K64 Click Shield + a few MikroE Click modules) and use it to teach the core embedded concepts that underlie automotive software: analog and digital signal acquisition, real-time processing, actuator control, and safety-aware system design. Together they cover the most common peripherals of the S32K3 family — ADC, GPIO, PWM, FlexIO, LPI2C, eMIOS — and expose students to the same tool-chain used by NXP customers: S32 Design Studio 3.6.5, the S32K3 Real-Time Drivers (RTD), the Application Code Hub (ACH), and the underlying Automotive Software Package. Learning philosophy — Eat-Sleep-Code-Repeat The whole workshop series is designed around the Eat-Sleep-Code-Repeat initiative — a learn-by-doing culture where students continuously iterate on real hardware, break things, fix them, refactor, and re-flash until the concepts stick. Every module is small enough to be completed in one lab session, yet rich enough to leave room for extensions (state machines, filtering, CAN networking, closed-loop control, safety fall-backs). Concepts covered across the series Analog sensing: potentiometers, force sensors, resistor-ladder buttons → ADC conversion, scaling, debouncing. Digital I/O: GPIO input handling (buttons, switches), GPIO output sequencing (stepper coils). Actuation: PWM-based motor speed control (DC motors, fans), PWM-based servo positioning, WS2812 LED driving through FlexIO. Communication: I²C configuration of external PWM drivers (Servo Click / PCA9685). Control patterns: continuous mapping, threshold-based decisions, state machines, safety interlocks. Automotive concepts: Body Control Module (BCM) behavior, functional safety (ISO 26262), fail-safe defaults, redundancy considerations. What this article gives you Each of the next five sections provides a short summary of one module — what it demonstrates, which hardware it uses, which peripherals are involved, and a direct link to the full detailed workshop article. Students should read this page first to understand where each module fits in the bigger picture, then dive into the individual articles for step-by-step instructions.   2. Vehicle Lighting Control   The Lights module implements a simplified automotive lighting system that mirrors the behavior of a real vehicle Body Control Module. Six buttons on the Analog Key Click command different lighting functions — low beam, high beam, left/right turn signals, brake lights, and hazard lights — all displayed in real time on a 16-LED 4x4 RGB Click matrix. Key learning points Multi-button decoding on a single ADC channel (resistor-ladder input). Software debouncing and command decoding. Driving WS2812 LEDs through FlexIO (precise sub-microsecond timing without CPU load). BCM safety interlocks: high beam requires low beam ON; hazards synchronize left + right turn signals; high beam state preserved between blink cycles. Peripherals used: ADC0, FlexIO, GPIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference project:Automotive Lighting Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community Demo: Vehicle Lighting Control on FRDM-A-S32K344 Automotive relevance: lighting is one of the most safety-critical driver-visibility functions in modern vehicles — this module teaches how a real BCM manages dependencies, blinking patterns, and fail-safe defaults.   3. Brake Status Monitoring   The Brakes module implements a simplified brake status monitoring system where a Force Click sensor simulates the driver's brake-pedal pressure. As pressure increases, the ADC value grows and the application progressively lights up the 4x4 RGB Click LEDs in green → yellow → orange → red, providing immediate visual feedback of the current braking level. Key learning points Continuous analog sensor acquisition through ADC. Threshold-based decision logic: converting a raw ADC value into discrete alert levels. Driving the RGB LED matrix through FlexIO to reflect the current system state. Introduction to real-time monitoring and safety-oriented visual feedback. Peripherals used: ADC0, FlexIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference project: Automotive Brake Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community Demo: Brake Status Monitoring on FRDM-A-S32K344 Automotive relevance: brake status is a core input for many downstream ECUs (ABS, ESC, hill-hold, brake lights). This module teaches the fundamental pattern of sensor → threshold → visual/electrical output that appears everywhere in automotive software.   4. Assisted Steering Control   The Steering module demonstrates a simplified Electric Power Steering (EPS) / steer-by-wire concept. A POT Click potentiometer simulates the steering-wheel angle; the MCU reads it through ADC, scales it linearly, and generates a PWM command through the Servo Click (configured over I²C) that positions a Micro Servo SG 180° in real time. Key learning points Analog input scaling and linear mapping (ADC range → servo angle range). Using an external PWM controller configured over I²C (LPI2C1) — a common embedded pattern that offloads timing-critical work. Working with the Output Enable (OE) pin for safe-stop behavior. Understanding the actuation chain sensor → MCU → PWM → actuator. Peripherals used: ADC0, LPI2C1, GPIO. Boards: FRDM-A-S32K312 or FRDM-A-S32K344. Reference projects: Automotive Steering Control Using FRDM-A-S32K3XX Microcontrollers - NXP Community Demo: PWM-Based Steering Control on FRDM-A-S32K344 Automotive relevance: steering is a strictly safety-relevant function (ISO 26262 typically classifies it as ASIL C or D). This module introduces the concepts behind EPS and steer-by-wire and lays the foundation for future work with redundant sensors and fault detection.   5. Vehicle Comfort Control   The Comfort module implements two independent comfort functions typical of vehicle body electronics: cabin cooling (a 5 V fan driven through a DC Motor 2 Click using PWM) and electric window control (a NEMA17 stepper motor driven through an H-Bridge Click using full-step GPIO sequencing). On-board push-buttons act as the driver's HVAC and window switches. Key learning points PWM motor speed control (fan simulation). Stepper motor full-step sequencing (A → B → C → D and reverse) through four GPIO outputs. Handling multiple independent actuators from a single MCU without blocking. Introduction to window anti-pinch and other real BCM safety concepts. Peripherals used: GPIO, eMIOS (PWM). Boards: FRDM-A-S32K344 (only). Reference project: Automotive Comfort Control Using FRDM-A-S32K344 Microcontrollers - NXP Community Demo: Vehicle Comfort Control on FRDM-A-S32K344 Automotive relevance: comfort systems (HVAC, windows, mirrors, seats) form a huge share of modern body electronics. This module shows how one ECU can coordinate multiple actuators of different types (rotational-speed and positional) using the same S32K3 platform.   6. Transmission Control   The Transmission module demonstrates a continuous, proportional transmission control concept. A POT Click potentiometer represents the driver's acceleration command; the MCU samples it, applies linear scaling, and simultaneously drives two actuators: a Servo Click + Micro Servo that simulates the transmission selector position, and a DC Motor 2 Click + DC motor whose speed reflects the powertrain response. Key learning points Dual-actuator control from a single analog input (one MCU commands both servo angle and DC motor speed in parallel). Linear signal mapping to two different PWM ranges simultaneously. Combining I²C-configured PWM (Servo Click) and eMIOS-generated PWM (DC Motor 2 Click) in the same application. Understanding continuous vs. discrete control and how continuous mapping better mirrors real automotive behavior. Peripherals used: ADC0, LPI2C1, eMIOS. Boards: FRDM-A-S32K344 (only). Reference project: Automotive Transmission Control Using FRDM-A-S32K344 Microcontrollers - NXP Community Demo: Transmission Control on FRDM-A-S32K344 Automotive relevance: transmission control is part of the powertrain domain and requires deterministic response and safety-aware design. This module introduces the concepts and prepares students for more advanced topics such as closed-loop control, transmission-mode logic (P/R/N/D), and CAN networking with the engine ECU.   7. Conclusion   Together, these five modules give students a complete tour of what a modern Body Control Module, Chassis ECU, and Powertrain ECU actually do in a vehicle — from reading sensors and buttons, through processing and safety interlocks, to driving lights, motors, and actuators. Each module can be studied independently, but the real value emerges when they are viewed as pieces of one coherent picture: the same MCU family (S32K3), the same tool-chain (S32 Design Studio + Application Code Hub), the same hardware base (FRDM-A-S32Kxxx + FRDM-K64 Click Shield + MikroE Click modules), applied to five different automotive domains. The series is intentionally aligned with the Eat-Sleep-Code-Repeat philosophy: start with a working example, then experiment — add filtering, replace polling with interrupts, introduce a state machine, add CAN communication, or refactor for functional safety. Every extension is a step closer to the way production automotive software is actually written. Recommended learning path: Lights — simplest, teaches ADC, FlexIO and BCM logic. Brakes — introduces continuous sensor thresholds. Steering — adds I²C-controlled PWM and actuator positioning. Comfort — multi-actuator, dual-technology control (PWM + stepper). Transmission — combines everything into a proportional, dual-actuator system.   If you have questions, suggestions for improvement, or ideas for new modules that could extend this series, please leave a comment below — feedback from students and instructors is what keeps the workshops relevant and up to date.  
記事全体を表示
The course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.
記事全体を表示