This page will guide you through the attachment of the servo to the Freescale Cup chassis. The servo steers the vehicle and is controlled using
Pulse-width modulation .
(Click any image to enlarge)
Inside the kit are various mounting options for different servo manufacturers. Look for the bushing of the servo that you are using.
You will need the three pieces shown below. You will screw this into the servo.


Pieces are notched, so assembly is straight forward.


Remove the screw and black servo plate.


Mount the yellow servo plate assembly to the servo as shown below. Make sure to add the small yellow washer (pictured below) in between the servo plate and the screw.


Tighten well, a servo produces a good amount of torque and will slip if not tight.
Assemble the short arm.


Assemble the long arm.


Attach the short arm to the yellow bracket.

First, insert the bearing into the control arm. This allows the joint to flex and move.
Screw this assembly into the servo plate.


Attach the long arm to the yellow bracket.
Attach the motor mount blocks to the back of the servo on both sides.

Screw in the attachment blocks from the bottom of the car.

How do you know where zero position is on servo? Maybe small on servo bushing?
May have to adjust later.
Another word of wisdom: adjust the length of the arms before attaching to the servo.
I have the same question
You have to power up the servo, create some code to set it to your "zero" and then adjust the steering arms accordingly.
It says to have servo in 0 degrees before securing the arms. Shouldn't it be in neutral position (90 degrees) for the car to go straight?