H Bridege

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

H Bridege

H Bridege

Overview

Image Unavailable

An H-Bridge circuit has a control circuit, usually PWM, which then determines the switching of high-voltage supply to drive a current. Typical embedded H-Bridges can drive about 5A of current. In the case, of the Freescale Cup car the motors can sustain much more current resulting in more toque and faster speeds.

Performance Tuning Tips

1. You can place H-Bridges in parallel to balance the current load. For example, if you place two 5A (peak) H-Bridge outputs in parallel, the system can support up to 10A current.
2. Keep it Cool. H-Bridge's dissipate A LOT of heat. Heat = increases inefficiency of a semiconductor, so the better job you do keeping it cool, the better (and longer) it will work for you.

Operation Theory

This is the simplest H-bridge, where the four gates represent for transistors. By manipulating these gates and connecting the upper and lower terminals to a voltage supply, you can control the motor in all the behaviors as below.

H-Bridge States
Image Unavailable
ラベル(1)
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-12-2012 12:33 PM
更新者: