Formula SAE Electric Vehicles USA 2013 winner is the Brazilian team from UNICAMP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Formula SAE Electric Vehicles USA 2013 winner is the Brazilian team from UNICAMP

Formula SAE Electric Vehicles USA 2013 winner is the Brazilian team from UNICAMP

This past Tuesday June 25th, 2013, the UNICAMP E-Racing compete against 19 teams and won the first place with a score of 985 points of a total of 1000.

The car used an electric motor of 120 V and a chassis that weighted 250 kg (551.2 lbs). That allows the car with a charging time of 2 hours to be driving for 25 km (15.5 miles) and race up to speeds of 170 km/h (105.6 mph).

Check out this video of the car:

The official results:

http://www.sae.org/images/cds/selfservice/372162833_FSAE_EV_2013%20result.pdf

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎06-27-2013 02:03 PM
更新者: