Automotive Transmission Control Using FRDM-A-S32K344 Microcontrollers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Automotive Transmission Control Using FRDM-A-S32K344 Microcontrollers

Automotive Transmission Control Using FRDM-A-S32K344 Microcontrollers

1. Overview

 

The application demonstrates actuator control concepts commonly encountered in automotive transmission systems using the FRDM-A-S32K344 development platform. The application showcases how analog input acquisition, signal processing, and actuator control can be combined to emulate the behavior of an automotive transmission control module.

The solution is based on an Application Code Hub example designed for the FRDM-A-S32K344 platform.

Transmission Control Module On FRDM-A-S32K344 

The demonstration uses a potentiometer as the primary input device, representing the driver's throttle command. The analog signal is sampled using the ADC peripheral and fed into a transmission model that simulates vehicle speed, automatically selects one of six forward gears or neutral, and estimates engine RPM. The current gear is physically indicated by a servo motor, while a DC motor reflects the throttle input through a variable PWM duty cycle, emulating the drivetrain response of a real vehicle.
 
The example highlights the interaction between analog sensing, ADC conversion, transmission control algorithms, I²C communication, PWM generation, and actuator control commonly found in automotive embedded systems.
 
More than a technical course, this program embodies the Eat-Sleep-Code-Repeat approach to learning, where students learn by doing. By repeatedly designing, coding, testing, and refining automotive embedded applications on real hardware platforms, participants build both practical skills and the confidence needed to tackle real-world engineering challenges.

 

2. Learning Scope

 

This article focuses on both practical implementation and core embedded system concepts:

  • Analog signal acquisition using ADC
  • Potentiometer-based continuous control inputs
  • PWM generation using the eMIOS peripheral
  • I²C communication with an external PWM controller
  • Servo motor position control through an external PWM driver
  • DC motor speed control with a dead-band region
  • Automatic gear selection with shift hysteresis
  • Engine RPM estimation and smoothing
  • Real-time embedded control loops running at a fixed update rate
  • Signal mapping and actuator response
The example provides a practical introduction to automotive control systems where continuous sensor values drive actuator behavior through a simulated transmission model.

 

3. System Architecture

 

The system follows a typical embedded control structure organised around a periodic control loop:

  • Input: Analog throttle signal from the potentiometer
  • Processing: S32K3 microcontroller running the transmission model (vehicle speed, gear selection, RPM)
  • Output: Servo motor position (via I²C to an external PWM controller) and DC motor speed (via eMIOS PWM)

Functional Flow

  1. The potentiometer voltage is sampled by the ADC and converted into a throttle command
  2. The MCU updates the transmission model, computing the simulated vehicle speed and selecting the appropriate gear
  3. The current gear is sent to the external PWM controller through I²C, which positions the servo motor accordingly
  4. The DC motor speed is updated through an eMIOS PWM channel proportional to the throttle command
  5. The entire cycle repeats at a fixed update rate to keep the actuators synchronised
Transmission_Control_Architecture.pngTransmission Control Application Architecture

Transmission Control Application Architecture

4. Key Concepts

 

4.1 Control Principle

Unlike systems based on push buttons or digital switches, this implementation uses a continuous analog input signal. The potentiometer provides a variable voltage level that represents the driver's throttle command. This value is continuously monitored and converted into a digital representation using the ADC peripheral. The processed value feeds a transmission model that simulates vehicle speed, selects a gear, and estimates engine RPM, which are then translated into commands for the servo (gear display) and the DC motor (speed). This approach allows smooth transitions instead of abrupt state changes and better reflects real-world automotive control systems.

4.2 Analog Input Acquisition

The potentiometer acts as a variable voltage divider. As the potentiometer position changes, the output voltage changes continuously, the ADC acquires the voltage, and the MCU converts it into a throttle percentage. This value becomes the primary input variable for the transmission model. This process mirrors how many automotive sensors operate, where physical movement or operating conditions are converted into an analog voltage signal that must be processed by the control unit.

4.3 Servo Motor Control via I²C and External PWM Controller

Unlike the DC motor, the servo motor is not driven directly by an MCU PWM channel. Instead, the MCU sends I²C commands to an external PWM controller located on the Servo Click board, which in turn generates the PWM pulses required to position the servo shaft. The transmission model computes the current gear and provides it as an input; the MCU translates the gear number into a pulse-width value and sends it to the external controller. Each discrete gear position corresponds to a specific servo angle, so the servo acts as a physical gear indicator on a graduated scale.

4.4 PWM-Based DC Motor Control

The DC motor is driven directly by the MCU through the eMIOS peripheral, which generates the PWM signal required by the DC Motor 2 Click H-bridge driver. As the potentiometer value increases, the PWM duty cycle also increases, resulting in higher motor speed. When the throttle is at zero, the motor is stopped; above zero, the duty cycle is clamped to a minimum dead-band value (approximately 20 % of the full range) to guarantee reliable motor start-up, and then scales linearly up to full speed. This mirrors the response of a real drivetrain to a throttle input.

4.5 Automatic Gear Selection with Hysteresis

The transmission model implements six forward gears plus neutral. Rather than mapping the throttle directly to a gear, the model maintains an internal simulated vehicle speed, which increases when the throttle is applied and decreases when it is released. Gear selection is performed by comparing the vehicle speed against a set of predefined thresholds:

  • An upshift occurs when the simulated speed rises above the upper threshold of the current gear.
  • A downshift occurs when the speed drops below the lower threshold of the current gear.
  • The distance between the up and down thresholds forms a hysteresis band, preventing rapid oscillation between two gears when the speed hovers near a shift point.
  • When the throttle is held at zero for a sustained period, the model detects idle and gradually downshifts back to neutral, mirroring the behaviour of a real automatic gearbox.

4.6 Engine RPM Estimation

In parallel with gear selection, the model estimates an engine RPM value based on the throttle input and the currently engaged gear. On each gear change, the RPM is smoothly adjusted — decreasing on upshifts and increasing on downshifts — to reproduce the characteristic behaviour of an automatic transmission. This smoothing avoids abrupt jumps and gives a more realistic feel to the simulation.

4.7 Signal Mapping

The application transforms the continuous throttle input into two coordinated actuator commands: a discrete gear position displayed by the servo, and a continuous PWM level applied to the DC motor. The conceptual mapping is shown below.

Throttle Input Transmission State Servo Position (Gear Indicator) DC Motor Speed
0 % (idle) Neutral Rest position Stopped
Low 1st – 2nd gear Low-gear positions Dead-band minimum → low speed
Medium 3rd – 4th gear Mid-range positions Medium speed
High 5th – 6th gear High-gear positions Maximum speed

This mapping demonstrates how a continuous sensor input can be transformed into both a discrete state (gear) and a continuous actuator command (motor speed).

4.8 Data Flow at a Glance

Physical rotation of the potentiometer → analog voltage → ADC sample → throttle percentage → transmission model (vehicle speed, gear, RPM) → I²C command to the external PWM controller (servo position) and eMIOS PWM signal (DC motor speed). All stages are re-evaluated at a fixed update rate to keep the actuators synchronised. This direct chain from the student's hand to the actuators is the main educational value of the demo.

5. Hardware and Software Setup

 

Required Hardware

Component Image Purpose
FRDM-A-S32K344 FRDM-A-S32K344FRDM-A-S32K344
MCU platform used to run the transmission control application, execute the transmission model, and drive the connected peripherals through ADC, eMIOS PWM, and I²C.
FRDM K64 click shield                 frdm-k64-clickFRDM-K64 Click Shield expansion board
mikroBUS expansion adapter that connects Click modules to the FRDM board.
Servo Click                         servo-clickServo Click PWM driver module
Expansion board carrying an external PWM controller. It receives I²C commands from the MCU and generates the PWM pulses that drive the servo motor.
Micro Servo Motor SG 180°                         micro-servo-motor-sg-180-degreeMicro Servo SG 180 degree actuator
Actuator used to physically indicate the currently selected gear on a graduated scale.
DC Motor 2 Click  dc-motor2-clickDC Motor 2 Click full-bridge driver
Compact add-on board with a PWM-controlled, full-bridge brushed DC motor driver. It receives the eMIOS PWM signal directly from the MCU.
DC Motor                      DC MotorDC Motor
Simulates the vehicle drivetrain speed, reflecting the throttle input applied by the user.
USB-C cable —
Provides power and enables programming and debugging.

 

The example application demonstrates how these peripherals are connected to the MCU pins and used to simulate a complete transmission control chain, from throttle input to gear indication and drivetrain speed.

 

Transmission Control Full Setup on FRDM-A-S32K344
Transmission Full SetupTransmission Full Setup

 

The hardware configuration allows simultaneous control of a position actuator (servo motor driven through I²C) and a speed-controlled actuator (DC motor driven through eMIOS PWM).

Software Environment

6. Implementation Guide

 

Step Action Sub-steps Expected Result
1 Import the Project
  • Open S32 Design Studio
  • Select “Import project from Application Code Hub”
  • Search for transmission control example
  • Use the GitHub link for automatic configuration
  • Select main branch
  • Import project
Project appears in workspace
2 Build the Application
  • Compile the project
  • Check for errors
  • Confirm SDK component management
Successful build with no errors
3 Connect Hardware
  • Connect the board via USB-C
  • Attach FRDM K64 Click Shield, Servo Click and DC Motor 2 Click
  • Wire the servo motor, DC motor and potentiometer
  • Verify wiring before powering the system
Board powers up and is detected by IDE
4 Flash and Run
  • Program the MCU
  • Start execution
Application runs continuously
5 Functional Validation
  • Rotate the potentiometer
  • Observe the servo pointer moving between the gear positions
  • Observe the DC motor speed changing proportionally to the throttle
  • Release the potentiometer and observe the transmission gradually downshifting back to neutral
Gear indicator and motor speed respond consistently to throttle changes

 

7. Signal Behavior and Control Logic

 

The following diagram illustrates how the transmission model selects the current gear based on the simulated vehicle speed, applying a hysteresis band to prevent frequent shifting around each threshold.
 

Transmission_Gear_Selection.png

The transmission continuously compares the simulated vehicle speed against a set of predefined speed thresholds, one per gear. An upshift occurs when the vehicle speed rises above the upper threshold of the current gear (blue lines), while a downshift occurs only when the speed drops below the lower threshold of that gear (red dashed lines). The distance between the two thresholds forms a hysteresis band that prevents rapid oscillation between adjacent gears when the vehicle speed hovers near a shift point. When the throttle is held at zero for a sustained period, the transmission detects idle and gradually downshifts back to neutral, mirroring the behaviour of a real automatic gearbox.

 

8. Troubleshooting

 

Issue Possible Actions
Board Not Detected
  • Verify USB connection
  • Check drivers
  • Restart IDE
DC Motor Not Responding
  • Check eMIOS PWM configuration
  • Verify motor driver wiring and external power supply
  • Confirm code execution
Servo Not Moving
  • Check I²C wiring (SDA / SCL) and pull-up resistors
  • Verify that the external PWM controller is powered
  • Confirm the servo is connected to the correct channel and powered by 5 V
Incorrect Behavior
  • Validate the ADC input range
  • Inspect GPIO configuration for motor direction pins
  • Verify transmission control logic implementation
Unstable / Jittery Output
  • Add software filtering on ADC readings
  • Check power supply stability
  • Verify grounding between motor drivers and MCU

 

9. Extending the Application

 

The application can be enhanced by adding:

Closed-Loop Control

  • Integrate feedback sensors to dynamically adjust actuator outputs

  • Compare commanded vs. actual position/speed for corrective action

Additional Transmission Modes

  • Extend the current six-gear + neutral model with Park and Reverse modes for a full PRND emulation

  • Map potentiometer regions or dedicated inputs to specific transmission states

Safety Functions

  • Implement input plausibility checks on the throttle signal

  • Add fault monitoring and safe-state transitions in case of sensor or actuator failure

CAN Communication

  • Transmit gear, RPM, and speed information over CAN or CAN FD networks

  • Integrate with larger automotive powertrain systems

Continuous Versus Discrete Control

  • Compare button-based (discrete) and potentiometer-based (continuous) input styles

  • Emulate electronic throttle control, position sensing, or actuator positioning applications

10. Safety Context

 

Transmission control is part of vehicle motion systems, requiring:

  • Reliable signal processing

  • Deterministic control behavior

  • Safety-aware design

In production systems:

  • Redundant checks are implemented

  • Fault detection is mandatory

  • Standards such as ISO 26262 apply

Automotive transmission control units also implement input plausibility checks and safe-state fallback strategies to prevent unintended gear engagement or actuator runaway.

11. Conclusion

 

This transmission control demonstration illustrates how the S32K344 platform can combine analog sensing, ADC conversion, I²C communication, PWM generation, and actuator control to implement a complete embedded control application.

Using a potentiometer as a continuous input source, the system processes the throttle signal through a transmission model with six forward gears plus neutral, hysteresis-based gear selection, and RPM estimation, and translates the result into real-time commands for both a servo motor (gear indicator) and a DC motor (drivetrain speed). The project provides practical insight into the operation of automotive control systems and serves as a foundation for more advanced transmission, actuator, and motion-control applications.

 

Result on FRDM-A-S32K344
Transmission resultTransmission result

 

The course provides a strong foundation for more advanced systems, including closed-loop feedback control, additional transmission modes, CAN communication, and safety-oriented designs typical of automotive transmission control modules.

評価なし
バージョン履歴
最終更新日:
‎07-03-2026 02:21 AM
更新者: