Automotive Comfort Control Using FRDM-A-S32K344 Microcontrollers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Automotive Comfort Control Using FRDM-A-S32K344 Microcontrollers

Automotive Comfort Control Using FRDM-A-S32K344 Microcontrollers

1. Overview

 

This module demonstrates how to implement a vehicle comfort control system using GPIO, PWM, and stepper motor sequencing on NXP S32K3 microcontrollers.

The application reads user inputs from push-buttons and translates them into two independent comfort functions: a DC motor that simulates a cabin cooling fan (regulated through PWM) and a stepper motor that simulates an electric window mechanism (driven through GPIO coil sequencing). Both actuators react in real time, mimicking how comfort body-control modules work in modern vehicles.

This example is based on the Application Code Hub demonstration for:

Vehicle Comfort Control for FRDM-A-S32K344

In this workshop, on-board push-buttons simulate the driver's comfort commands. When the student presses a button, the MCU reads the input through GPIO, decodes the requested action, and drives the associated actuator: a PWM duty cycle is generated for the DC Motor 2 Click (regulating the fan speed), or a full-step coil sequence is generated through GPIO outputs to the H-Bridge Click (moving the NEMA17 stepper motor up or down).

Beyond the technical implementation, the course serves as a foundation for the Eat-Sleep-Code-Repeat learning initiative, encouraging a hands-on approach where students continuously learn, develop, test, and improve automotive embedded applications using real hardware and practical examples.

 

2. Learning Scope

 

After completing this course, participants should be able to:
 
  • Understand a basic vehicle comfort control system and the ideas behind HVAC regulation and electric window control.
  • Use on-board push-buttons as simulated driver comfort commands.
  • Read digital inputs using the GPIO peripheral and understand debouncing considerations.
  • Generate PWM signals to regulate DC motor speed (fan simulation).
  • Implement a full-step drive sequence (A → B → C → D) to control a stepper motor.
  • Configure the DC Motor 2 Click and H-Bridge Click boards over the mikroBUS interface.
  • Recognize the actuation data flow: user input → MCU processing → PWM / GPIO actuation.
  • Import, build, flash, and debug an ACH project in S32 Design Studio 3.6.5.
  • Understand why comfort functions are relevant in modern automotive body electronics.

3. System Architecture

 

The three elements capture exactly the basic idea of the system in the demo:

  • Input: Push-buttons (on-board buttons simulate driver comfort commands)
  • Processing: S32K3 MCU (reads GPIO, decodes the command, drives the correct actuator)
  • Output: Dual actuation (DC motor via PWM for the fan, stepper motor via GPIO sequencing for the window)

This matches the classic flow of an embedded body-control system: user input → processing → actuator.

Functional Flow

The system operates continuously as follows:

  1. The user presses a button that corresponds to a comfort action
  2. The GPIO peripheral reads the button state
  3. The application decodes the command (fan control or window movement)
  4. Depending on the command, the MCU generates either a PWM signal or a stepper coil sequence
  5. The DC motor changes speed, or the stepper motor rotates in the requested direction

This loop runs continuously to ensure real-time comfort control.

Comfort_Control_Application.pngVehicle Comfort Control Application Architecture

Vehicle Comfort Control Application Architecture

4. Key Concepts

 

4.1 GPIO (General-Purpose Input/Output)

The push-buttons on the FRDM-A-S32K344 board are connected to GPIO input pins. The MCU polls (or reads on interrupt) the pin state and interprets a logic transition as a user command. GPIO is also used as output for the stepper motor coil control signals, driving the H-Bridge Click inputs. GPIO handling is the foundation of automotive user-interface processing — used for buttons, switches, ignition detection, and many others.

4.2 PWM — Pulse-Width Modulation and Fan Speed Control

PWM switches a digital output on and off at a fixed frequency, varying the duty cycle (the fraction of time the signal is high). A DC motor interprets the average voltage produced by this PWM as a proportional rotational speed. In this demo, the S32K344 generates PWM on a mikroBUS pin that drives the DC Motor 2 Click, which in turn powers the 5 V fan motor. Increasing the duty cycle increases fan speed; decreasing it slows the fan down — a typical pattern used in cabin ventilation and HVAC systems.

4.3 DC Motor Direction and H-Bridge Concept

The DC Motor 2 Click integrates an H-Bridge driver that can be configured for forward, reverse, brake, or coast modes. The MCU controls the direction pins and applies PWM on the enable input to regulate speed. This is exactly the same principle used in real automotive fan modules, where a low-side or full-bridge driver is switched at kilohertz frequency to obtain smooth speed control without dissipating power in a series resistor.

4.4 Stepper Motor Full-Step Sequencing

A stepper motor like the NEMA17 rotates in fixed angular increments (typically 1.8° per step) when its coils are energized in the correct order. The MCU generates a repeating four-phase pattern (A → B → C → D) on four GPIO pins connected to the H-Bridge Click. Reversing the sequence (D → C → B → A) reverses the direction. The step frequency directly determines rotation speed, and counting the number of steps gives an open-loop position estimate — the exact behavior needed to simulate an electric window moving up or down.

4.5 Push-Buttons as Comfort Commands

The on-board buttons are a simplified, safe stand-in for the physical HVAC and window switches found in a real vehicle. The student presses them by hand, the GPIO state changes, the MCU decodes the command, and the corresponding actuator reacts. This isolates the student from real body-electronics wiring while preserving the full software logic.

4.6 Data Flow at a Glance

Button press → GPIO input → command decoding → selection of actuator (fan or window) → PWM duty cycle update or stepper coil sequence advance → motor response. This direct chain from the student's finger to the actuator shaft is the main educational value of the demo.

5. Hardware and Software Setup

 

Required Hardware

Component Image Purpose
FRDM-A-S32K344 FRDM-A-S32K344FRDM-A-S32K344
MCU platform used to run the comfort control application and drive the connected peripherals.
FRDM-K64 Click Shield FRDM K64 click shieldFRDM K64 click shield
mikroBUS expansion board used to connect Click modules to the FRDM platform.
DC Motor 2 Click DC Motor 2 ClickDC Motor 2 Click
H-Bridge driver board used to control DC motor speed and direction via PWM.
H-Bridge Click H-Bridge ClickH-Bridge Click
Dual H-Bridge driver used to sequence the stepper motor coils.
5 V Fan Motor 5V Fan Motor5V Fan Motor
Actuator used to simulate the vehicle cabin cooling fan controlled through PWM.
Stepper Motor NEMA17 Stepper Motor Nema17Stepper Motor Nema17
Actuator used to simulate the electric window mechanism through step sequencing.
USB-C  —
Provides power and enables programming and debugging of the system.

 

The example application demonstrates how these peripherals are connected to the MCU pins and used to simulate cabin cooling and electric window control.

 

Vehicle Comfort Control Full Setup on FRDM-A-S32K344
Comfort Full SetupComfort Full Setup

 

Software Environment

6. Implementation Guide

 

Step Action Sub-steps Expected Result
1 Import the Project
  • Open S32 Design Studio
  • Select “Import project from Application Code Hub”
  • Search for the vehicle comfort control demo
  • Use the GitHub link for automatic configuration
  • Select main branch
  • Import project
Project successfully appears in workspace
2 Build the Application
  • Right-click project
  • Select “Update Code and Build Project”
  • Confirm SDK component management
Build completes with no errors and generates .elf file
3 Connect Hardware
  • Connect USB cable and external 12 V supply
  • Attach FRDM-K64 Click Shield, DC Motor 2 Click and H-Bridge Click
  • Wire the 5 V fan motor and NEMA17 stepper motor
  • Verify wiring before powering the system
Board is powered and detected by IDE
4 Flash and Run
  • Open Debug Configurations
  • Select “debug_flash_pemicro”
  • Start debugging
Application runs continuously
5 Functional Validation
  • Press the fan control buttons
  • Observe DC motor speed change
  • Press the window up/down buttons
  • Observe stepper motor movement and direction
Fan speed and window motion follow user commands in real time

 

7. Signal Behavior and Control Logic

 

The Vehicle Comfort Control application drives two independent actuators from a single S32K344 MCU: a DC fan motor controlled through a PWM signal for cooling, and a stepper motor controlled through a 4-channel GPIO sequence for electric window movement. User inputs (SW2 and SW3) are read by the MCU, which then generates the appropriate signal type for each actuator. The two diagrams below describe the signal behavior and control logic for each subsystem.

 

7.1 Cooling System – Fan Speed Control (PWM)

 

Comfort_Fan_PWM.png

Figure: Fan speed control mapping. The MCU generates a PWM signal on the EMIOS channel to drive the DC fan motor through the DC MOTOR 2 Click board. Each SW2 press increments the duty cycle by one step (0 % → 33 % → 67 % → 100 %) and each SW3 press decrements it, so fan speed is directly proportional to duty cycle. Duty Counts represent the raw PWM compare values (period = 20000 counts). When the fan is fully stopped, the TB6593FNG driver is automatically put into low-power sleep mode to prevent wasted current through the windings.

 

7.2 Window System – Stepper Motor Full-Step Sequencing

 

Direction Step # Coil A (PTA13) Coil B (PTD0) Coil C (PTA3) Coil D (PTC10) Active Pair
UP
(SW2 pressed)
1 ON OFF ON OFF AC
2 OFF ON ON OFF BC
3 OFF ON OFF ON BD
4 ON OFF OFF ON AD
DOWN
(SW3 pressed)
1 ON OFF OFF ON AD
2 OFF ON OFF ON BD
3 OFF ON ON OFF BC
4 ON ON OFF OFF AC

Table: Stepper motor full-step sequencing for window control. The MCU drives the stepper motor through four GPIO lines connected to the H-Bridge Click board, using dual-coil activation (two coils energised per step) to maximise torque. Pressing SW2 executes the Up sequence AC → BC → BD → AD (window moves up), while SW3 executes the reversed Down sequence AD → BD → BC → AC (window moves down). Each press advances the motor by one full step with a 3 ms delay, and the coil pair remains energised as long as the button is held. When no button is pressed, all coils are de-energised to prevent motor winding overheating during idle periods.

 

8. Troubleshooting

 

Issue Possible Actions
Board Not Detected
  • Check USB cable and drivers
  • Verify debugger connection
  • Restart IDE
Fan Does Not Spin
  • Verify PWM configuration and duty cycle
  • Check DC Motor 2 Click wiring and enable pins
  • Ensure the 5 V motor supply is present
Stepper Not Moving
  • Verify GPIO output configuration for coil pins
  • Check H-Bridge Click wiring and coil order
  • Confirm the step delay is not too short (motor stalls)
Stepper Rotates Wrong Direction
  • Invert the coil sequence in software (A→B→C→D vs D→C→B→A)
  • Swap one coil pair on the H-Bridge output
Buttons Not Responding
  • Verify GPIO input configuration and pull-up/pull-down
  • Add software debouncing
  • Check that the correct button pins are mapped

 

9. Extending the Application

 

The basic implementation can be extended in several ways:

Feedback-Based Control

  • Add temperature or Hall-effect sensors for closed-loop fan speed regulation

  • Add end-stop switches or encoders for accurate window position tracking

Automatic Comfort Modes

  • Implement predefined climate or ventilation profiles

  • Trigger comfort actions based on sensor thresholds

CAN Communication

  • Enable communication with other vehicle ECUs (e.g., HVAC master, door module)

  • Receive comfort commands over the vehicle network

Diagnostic Functions

  • Add fault detection for stuck motors, over-current or open loads

  • Expose diagnostic status via LEDs or debug UART

Position Memory

  • Store and restore window or fan positions in non-volatile memory

  • Recall the last comfort state after each power-up

State Machine Implementation A more advanced approach is to implement a state machine:

  • Idle

  • Active

  • Fault

10. Safety Context

 

This example reflects key automotive principles:

  • Continuous monitoring of driver commands

  • Immediate response to control signals

  • Reliable actuator control for both speed and position

In real systems:

  • Redundancy is required for safety-relevant functions (e.g., anti-pinch on windows)

  • Fault detection mechanisms are implemented (over-current, stall, over-temperature)

  • Systems must comply with ISO 26262 (functional safety standard) where applicable

Modern comfort modules also implement anti-pinch protection on power windows, ensuring the motor stops or reverses when an obstruction is detected — a safety-critical requirement for real vehicles.

11. Conclusion

 

This module demonstrates how a simple embedded system can implement vehicle comfort control using GPIO inputs, PWM outputs, and stepper motor sequencing on the S32K344 platform.

It shows how:

  • Digital user inputs are acquired through GPIO

  • Commands are decoded and processed in real time

  • A DC motor is controlled using PWM for smooth speed regulation

  • A stepper motor is controlled using a full-step coil sequence for precise positioning

 

Result on FRDM-A-S32K344
Comfort ResultComfort Result

 

The course provides a strong foundation for more advanced systems, including feedback-based control, CAN networking, diagnostics, and safety-oriented designs typical of automotive body-control modules.

評価なし
バージョン履歴
最終更新日:
‎07-02-2026 05:14 AM
更新者: