This article demonstrates how to implement a brake status monitoring system using NXP S32K3 microcontrollers. The solution is based on Application Code Hub examples for S32K344 and S32K312 platforms and showcases how real-time sensor data can be used to detect braking events and trigger visual feedback.
This is based on the following Application Code Hub demonstrations:
This article covers both practical implementation and core embedded concepts, including:
The application is built around a simple but representative embedded system:
Brake Monitoring Application Architecture
Sensors typically output analog values that must be digitized for processing. The ADC periodically samples this signal and produces a digital representation used by the application logic.
Typical interpretation:
The system continuously reads sensor data and reacts immediately. This is essential in automotive contexts where delayed responses may impact system behavior.
The LED output reflects the system state:
In extended implementations, multiple states or patterns can be used.
Required Hardware
| Component | Image | Purpose |
|---|---|---|
| FRDM-A-S32K312 |
Alternative MCU platform used to run the brake application and process brake inputs.
|
|
| FRDM-A-S32K344 |
Alternative MCU platform used to run the brake application and control connected peripherals.
|
|
| FRDM K64 click shield | |
mikroBUS expansion adapter that connects Click modules to the FRDM board
|
| Force Click (or similar analog sensor module) | |
Simulates the brake pedal by producing an analog signal proportional to applied pressure
|
| 4x4 RGB Click (LED output) | |
Displays real-time brake status through colored LED patterns (green → yellow → orange → red)
|
| USB cable / power supply | — |
Powers the FRDM board and provides debug connectivity to the PC
|
The example applications demonstrate how these peripherals are connected to the MCU pins and used to simulate brake inputs and outputs.
| Brake Control Monitoring on FRDM-A-S32K312 | Brake Control Monitoring on FRDM-A-S32K344 |
|---|---|
| Step | Action | Sub-steps | Expected Result |
|---|---|---|---|
| 1 | Import the Project |
|
Project is successfully loaded into the workspace |
| 2 | Build the Application |
|
No compilation errors |
| 3 | Connect Hardware |
|
Board is powered and detected by the IDE |
| 4 | Flash and Run |
|
Application runs continuously |
| 5 | Functional Validation |
|
LED activates when braking condition is detected |
The application relies on threshold-based decision logic:
| Issue | Possible Actions |
|---|---|
| Board Not Detected |
|
| No Output Response |
|
| Incorrect Sensor Readings |
|
The basic implementation can be extended in several ways:
A more advanced approach is to implement a state machine:
Although simplified, this application reflects concepts used in automotive safety systems:
In real systems, additional mechanisms are required:
This example demonstrates how a simple embedded application can model a real-world automotive use case. By combining ADC input, real-time processing, and GPIO output, it highlights the core principles behind monitoring functions in automotive ECUs.
| Result on FRDM-A-S32K312 | Result on FRDM-A-S32K344 |
|---|---|
The course provides a foundation for more advanced designs, including multi-state logic, filtering techniques, and safety-focused extensions.