1. Overview
This article demonstrates how to implement a brake status monitoring system using NXP S32K3 microcontrollers. The solution is based on Application Code Hub examples for S32K344 and S32K312 platforms and showcases how real-time sensor data can be used to detect braking events and trigger visual feedback.
This is based on the following Application Code Hub demonstrations:
The application simulates braking conditions using a sensor input and provides immediate system response via an LED indicator. Such systems are commonly used in automotive environments to improve system awareness and support safety-related functionality.
Beyond teaching technical concepts, the course promotes the Eat-Sleep-Code-Repeat methodology as a core learning principle. Students are encouraged to continuously explore, implement, test, and enhance automotive embedded applications using real hardware and practical examples, reinforcing knowledge through repetition, experimentation, and hands-on problem solving.
2. Learning Scope
This article covers both practical implementation and core embedded concepts, including:
- Reading analog signals using ADC
- Processing real-time signals
- Controlling outputs using GPIO
- Implementing decision logic based on thresholds
- Understanding signal flow in embedded systems
3. System Architecture
The application is built around a simple but representative embedded system:
- Input: Analog sensor (force / brake simulation)
- Processing: S32K3 microcontroller
- Output: LED indicator
Functional Flow
- The sensor generates an analog signal proportional to applied force
- The ADC converts the analog signal into a digital value
- The software evaluates the value against defined thresholds
- The system updates the output (LED) based on braking state
Brake Monitoring Application Architecture
4. Key Concepts
Analog Signal Acquisition (ADC)
Sensors typically output analog values that must be digitized for processing. The ADC periodically samples this signal and produces a digital representation used by the application logic.
Typical interpretation:
- Low value → no braking activity
- High value → braking detected
Real-Time Signal Processing
The system continuously reads sensor data and reacts immediately. This is essential in automotive contexts where delayed responses may impact system behavior.
Output Control Using GPIO
The LED output reflects the system state:
- OFF → no braking detected
- ON → braking condition detected
In extended implementations, multiple states or patterns can be used.
5. Hardware and Software Setup
Required Hardware
| Component |
Image |
Purpose |
| FRDM-A-S32K312 |
FRDM-A-S32K312 |
Alternative MCU platform used to run the brake application and process brake inputs.
|
| FRDM-A-S32K344 |
FRDM-A-S32K344 |
Alternative MCU platform used to run the brake application and control connected peripherals.
|
| FRDM K64 click shield |
 |
mikroBUS expansion adapter that connects Click modules to the FRDM board
|
| Force Click (or similar analog sensor module) |
Force Click |
Simulates the brake pedal by producing an analog signal proportional to applied pressure
|
| 4x4 RGB Click (LED output) |
4X4 RGB Click |
Displays real-time brake status through colored LED patterns (green → yellow → orange → red)
|
| USB cable / power supply |
— |
Powers the FRDM board and provides debug connectivity to the PC
|
The example applications demonstrate how these peripherals are connected to the MCU pins and used to simulate brake inputs and outputs.
| Brake Control Monitoring on FRDM-A-S32K312 |
Brake Control Monitoring on FRDM-A-S32K344 |
Brake Control Monitoring on FRDM-A-S32K312 |
Brake Control Monitoring on FRDM-A-S32K344 |
Software Environment
- S32 Design Studio
- S32K3 Automotive Software Package
- Application Code Hub project import
6. Implementation Guide
| Step |
Action |
Sub-steps |
Expected Result |
| 1 |
Import the Project |
- Open S32 Design Studio
- Use “Import project from Application Code Hub”
- Locate the brake monitoring example
- Import and configure the project
|
Project is successfully loaded into the workspace |
| 2 |
Build the Application |
- Compile the project
- Resolve any dependency issues if needed
|
No compilation errors |
| 3 |
Connect Hardware |
- Connect the development board via USB
- Attach sensor and LED modules
- Ensure correct pin connections
|
Board is powered and detected by the IDE |
| 4 |
Flash and Run |
- Program the MCU
- Start execution
|
Application runs continuously |
| 5 |
Functional Validation |
- Apply pressure to the sensor
- Observe LED behavior
|
LED activates when braking condition is detected |
7. Signal Behavior and Threshold Logic
The application relies on threshold-based decision logic:
- If ADC value < threshold → no brake
- If ADC value ≥ threshold → brake active
Signal vs Threshold Diagram

8. Troubleshooting
| Issue |
Possible Actions |
| Board Not Detected |
- Verify USB cable and drivers
- Check debugger connection
- Restart IDE
|
| No Output Response |
- Validate GPIO configuration
- Check LED connections
- Confirm code execution
|
| Incorrect Sensor Readings |
- Verify ADC configuration
- Inspect sensor wiring
- Confirm scaling and thresholds
|
9. Extending the Application
The basic implementation can be extended in several ways:
Multi-Level Brake Detection
- Define multiple thresholds:
- Low → normal
- Medium → moderate braking
- High → emergency braking
Noise Filtering
- Apply software filtering to stabilize readings
- Avoid false triggering from sensor noise
Timing-Based Logic
- Add debounce or delay mechanisms
- Require sustained input before triggering
State Machine Implementation
A more advanced approach is to implement a state machine:
10. Safety Context
Although simplified, this application reflects concepts used in automotive safety systems:
- Continuous monitoring of input signals
- Immediate response to changes
- Clear indication of system state
In real systems, additional mechanisms are required:
- Redundancy
- Fault detection
- Compliance with safety standards (e.g., ISO 26262)
11. Conclusion
This example demonstrates how a simple embedded application can model a real-world automotive use case. By combining ADC input, real-time processing, and GPIO output, it highlights the core principles behind monitoring functions in automotive ECUs.
| Result on FRDM-A-S32K312 |
Result on FRDM-A-S32K344 |
Result on FRDM-A-S32k312 |
Result on FRDM-A-S32K344 |
The course provides a foundation for more advanced designs, including multi-state logic, filtering techniques, and safety-focused extensions.