DC Motors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DC Motors

1,629 次查看
Valeriu
Contributor I

Hello,

We want to participate this year at Freescale Cup, but using the old kit from last year. The problem is that the old kit have a broken motor, it's spins slower by 20%, so we have different cornering speeds depending on the direction.

We need 2 new motors, one as spare part, but to buy a whole kit just for this motors it's too expensive. Other solution is to buy from big distributors like Digikey, Mouser, Farnell, but they don't have anything similar (7.2V - 16000 rpm). Also I don't find this motor on the manufacturer site: STANDARD MOTOR - Powered by Source Technology Limited. Something similar I saw only on ebay: Metal Housing Round Shape Magnetic Micro Motor 16000rpm 0 7A 7 2V DC | eBay, but dimensions differs.

Can you provide a list of allowed motors from known companies that can be found in Europe, because DC motor is a very important part that is easy to broken when you start to run at high speed.

Second question:

2. The chassis can be modified, with some restrictions:

a. The footprint of the frame may not be altered

b. You may not change the distance between wheels

With this in mind, it is allowed to cut 2 cm of the frame in front of servo just to be easier to climb the slope?

Thanks

标记 (3)
0 项奖励
1 回复

1,295 次查看
FlavioStiffan
NXP Employee
NXP Employee

HHi Valeriu

i have a couple of spare motors from original make, please send me a shipping address via email at [email protected] and I will be able to help with this.

for the chassis, the rules are clear: not changing the footprint of frame clearly says that cutting a piece off for making it shorter is not allowed.