uboot to linux mapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot to linux mapping

1,543 Views
rashmikj
Contributor III

I am new to the linux environment. Can anyone explain which device tree file will be used for linux kernel for LS1046ARDB board as there are multiple device tree files in linux folder. Am using flex installer and LSDK.

0 Kudos
Reply
1 Reply

1,512 Views
ufedor
NXP Employee
NXP Employee

arch/arm64/boot/dts/freescale/

fsl-ls1046a.dtsi
fsl-ls1046a-rdb.dts
fsl-ls1046a-rdb-usdpaa.dts
fsl-ls1046a-rdb-sdk.dts
fsl-ls1046-post.dtsi

qoriq-qman-portals-sdk.dtsi
qoriq-bman-portals-sdk.dtsi
qoriq-dpaa-eth.dtsi
qoriq-fman3-0-6oh.dtsi
qoriq-fman3-0.dtsi
qoriq-fman3-0-1g-0.dtsi
qoriq-fman3-0-1g-1.dtsi
qoriq-fman3-0-1g-2.dtsi
qoriq-fman3-0-1g-3.dtsi
qoriq-fman3-0-1g-4.dtsi
qoriq-fman3-0-1g-5.dtsi
qoriq-fman3-0-10g-0.dtsi
qoriq-fman3-0-10g-1.dtsi

include/

dt-bindings/interrupt-controller/arm-gic.h
dt-bindings/thermal/thermal.h

0 Kudos
Reply