u-boot SMP Threads T2080RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot SMP Threads T2080RDB

1,937 Views
albertandreasjr
Contributor II

Using u-boot T2080RDB_SPIFLASH_config of version V2.0-1703.

The T2080 has 4 cores with two threads.  Will u-boot support having the 7 threads in the spin tables.  Right now it only has the 3 cores waiting on the spin tables.  (I removed addr, and r3 for brevity).

What it does now:

Running on cpu 0

    pir - 0x00000002
Running on cpu 0

    pir - 0x00000004
Running on cpu 0

   pir - 0x00000006

I would like:

Running on cpu 1

    pir - 0x00000001
Running on cpu 0

    pir - 0x00000002
Running on cpu 1

   pir - 0x00000003

....

Running on cpu 1

   pir - 0x00000007

I am doing this to get vxWorks Boot running in SMP with SMT mode, with a modified bootInit.s.

I would like to do :

cpu 1 release <_romInit> 1 1 2

cpu 2 release <_romInit> 8 1 2

cpu 3 release <_romInit> 9 1 2

cpu 4 release <_romInit> 10 1 2

cpu 5 release <_romInit> 11 1 2

cpu 6 release <_romInit> 18 1 2

cpu 7 release <_romInit> 19 1 2

Al

Labels (1)
0 Kudos
Reply
2 Replies

1,561 Views
bpe
NXP Employee
NXP Employee


What you want to do contradicts the requirements of ePAPR,
Sections 5.4.1, 5.5.2.2, thus not verified by NXP and most likely is
not implemented. Not sure this is an actual requirement by VxWorks
because threads are not fully independent CPUs in many aspects, for
instance, they don't have separate virtual address spaces. Suggest
contacting with VxWorks for clarifications.

Best Regards,

Platon

0 Kudos
Reply

1,561 Views
albertandreasjr
Contributor II

I figured it out.  I found a Linux checkin that gave me a hint.

https://lists.denx.de/pipermail/u-boot/2010-September/078097.html

"Some OSes require that secondary cores not be initialized when they are booted (eg VxWorks)."

So I left the cores in holdoff then allowed VxWorks to release the 7 threads
0 Kudos
Reply