t2080 processor using raw socket required to improve the throughput of ethernet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

t2080 processor using raw socket required to improve the throughput of ethernet

1,896 次查看
bhargavram
Contributor I

How to calculate bandwidth of ethernet in t2080 processor.

In t2080 processor using raw socket  required to improve the throughput of ethernet.

Tested using kernel 3.8 and "fsl_fman_ucode_t2080_r1.0_106_4_14" or "fsl_fman_ucode_t2080_r1.1_108_4_5" and getting only 11mbs(Full Duplex) with raw socket . Kindly provide a solution to improve ethernet throughput.

标签 (1)
0 项奖励
回复
2 回复数

1,779 次查看
alexander_yakov
NXP Employee
NXP Employee

Please refer to "Benchmark Reproducibility Guide" in our Linux SDK documentation:

https://nxp.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-B65DA9CC-28BD-4EAF-A5B1-A371291...


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,779 次查看
bhargavram
Contributor I

Its 11 MBPS(Mega Byte per Sec)

0 项奖励
回复