t2080 processor using raw socket required to improve the throughput of ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

t2080 processor using raw socket required to improve the throughput of ethernet

1,900 Views
bhargavram
Contributor I

How to calculate bandwidth of ethernet in t2080 processor.

In t2080 processor using raw socket  required to improve the throughput of ethernet.

Tested using kernel 3.8 and "fsl_fman_ucode_t2080_r1.0_106_4_14" or "fsl_fman_ucode_t2080_r1.1_108_4_5" and getting only 11mbs(Full Duplex) with raw socket . Kindly provide a solution to improve ethernet throughput.

Labels (1)
0 Kudos
Reply
2 Replies

1,783 Views
alexander_yakov
NXP Employee
NXP Employee

Please refer to "Benchmark Reproducibility Guide" in our Linux SDK documentation:

https://nxp.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-B65DA9CC-28BD-4EAF-A5B1-A371291...


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,783 Views
bhargavram
Contributor I

Its 11 MBPS(Mega Byte per Sec)

0 Kudos
Reply