t1040d4rdb cannot get past runlevel request

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

t1040d4rdb cannot get past runlevel request

2,360 次查看
WmBAnderson
Contributor I

I have built a Yocto full image load for a t1040d4rdb following the QorIQ SDK v2.0-1703 Documentation.

using these commands I have gotten the image to almost load;

setenv ethact FM1@DTSEC4

ping 192.168.1.95

Using FM1@DTSEC4 device

host 192.168.1.95 is alive

Upload the U-BOOT:

tftp 0x1000000 u-boot-t1040d4rdb-64b.bin

protect off 0xebf40000 +$filesize

erase 0xebf40000 +$filesize

cp.b 0x1000000 0xebf40000 $filesize

protect on 0xebf40000 +$filesize

Upload the RCW:

tftp 0x1000000 rcw/t1040d4rdb/RR_P_66/rcw_1400MHz.bin

protect off 0xec000000 +$filesize

erase 0xec000000 +$filesize

cp.b 0x1000000 0xec000000 $filesize

protect on 0xec000000 +$filesize

Upload the microcode FMAN

tftp 0x1000000 fsl_fman_ucode_t1040_r1.1_106_4_18.bin

protect off 0xEBF00000 +$filesize

erase 0xEBF00000 +$filesize

cp.b 0x1000000 0xEBF00000 $filesize

protect on 0xEBF00000 +$filesize

saveenv

Switch to Bank 4

cpld reset altbank

setenv ethact FM1@DTSEC4

setenv initrd_high 0xffffffff

setenv bootargs ‘root=/dev/ram rw console=ttyS0,115200 ramdisk_size=10000000 log_buf_len=128K’

saveenv

tftp 0x1000000 uImage-t1040d4rdb-64b.bin

tftp 0x2000000 uImage-t1040d4rdb.dtb

tftp 0x3000000 fsl-image-full-t1040d4rdb-64b-20201123203234.rootfs.ext2.gz.u-boot

bootm 0x1000000 0x3000000 0x2000000

However I have not been able to get past the runlevel request and the u-boot log has several issues that look suspicious.  Is there a better build that can support my unmodified t1040d4rdb?

All assistance is most appreciated.

Bill

=> bootm 0x1000000 0x3000000 0x2000000

WARNING: adjusting available memory to 30000000

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-4.1.35-rt41

   Image Type:   PowerPC Linux Kernel Image (gzip compressed)

   Data Size:    5476290 Bytes = 5.2 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Loading init Ramdisk from Legacy Image at 03000000 ...

   Image Name:   fsl-image-full-t1040d4rdb-64b-20

   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)

   Data Size:    416517853 Bytes = 397.2 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 02000000

   Booting using the fdt blob at 0x2000000

   Uncompressing Kernel Image ... OK

   Loading Device Tree to 02fe4000, end 02fffe86 ... OK

Warning: MAC address for l2switch not found

Reserved memory: initialized node bman-fbpr, compatible id fsl,bman-fbpr

Reserved memory: initialized node qman-fqd, compatible id fsl,qman-fqd

Reserved memory: initialized node qman-pfdr, compatible id fsl,qman-pfdr

Reserved memory: initialized node pme-pdsr, compatible id fsl,pme-pdsr

Reserved memory: initialized node pme-sre, compatible id fsl,pme-sre

Using CoreNet Generic machine description

MMU: Supported page sizes

         4 KB as direct

      4096 KB as direct

     16384 KB as direct

     65536 KB as direct

    262144 KB as direct

   1048576 KB as direct

MMU: Book3E HW tablewalk not supported

Found initrd at 0xc000000003000040:0xc00000001bd38f1d

bootconsole [udbg0] enabled

CPU maps initialized for 1 thread per core

Starting Linux PPC64 #1 SMP Sat Nov 21 09:40:19 EST 2020

-----------------------------------------------------

ppc64_pft_size    = 0x0

phys_mem_size     = 0x200000000

dcache_line_size  = 0x40

icache_line_size  = 0x40

cpu_features      = 0x00180400581802c0

  possible        = 0x00180480581802c0

  always          = 0x00180400581802c0

cpu_user_features = 0xcc008000 0x08000000

mmu_features      = 0x000a0010

firmware_features = 0x0000000000000000

-----------------------------------------------------

 <- setup_system()

Linux version 4.1.35-rt41 (bill@bill-Precision-M4700) (gcc version 4.9.2 (GCC) ) #1 SMP Sat Nov 21 09:40:19 EST 2020

CoreNet Generic board

Zone ranges:

  DMA      [mem 0x0000000000000000-0x000000007fffffff]

  DMA32    empty

  Normal   [mem 0x0000000080000000-0x00000001ffffffff]

Movable zone start for each node

Early memory node ranges

  node   0: [mem 0x0000000000000000-0x00000001ffffffff]

Initmem setup node 0 [mem 0x0000000000000000-0x00000001ffffffff]

MMU: Allocated 2112 bytes of context maps for 255 contexts

PERCPU: Embedded 17 pages/cpu @c0000001fe600000 s30488 r0 d39144 u262144

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 2068480

Kernel command line: ‘root=/dev/ram rw console=ttyS0,115200 ramdisk_size=10000000 log_buf_len=128K’

log_buf_len: 131072 bytes

early log buf free: 12300(75%)

PID hash table entries: 4096 (order: 3, 32768 bytes)

Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes)

Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes)

Sorting __ex_table...

Memory: 7689564K/8388608K available (8484K kernel code, 1204K rwdata, 3212K rodata, 388K init, 766K bss, 699044K reserved, 0K cma-reserved)

Hierarchical RCU implementation.

        Additional per-CPU info printed with stalls.

NR_IRQS:512 nr_irqs:512 16

mpic: Setting up MPIC " OpenPIC  " version 1.2 at ffe040000, max 4 CPUs

mpic: ISU size: 512, shift: 9, mask: 1ff

mpic: Initializing for 512 sources

clocksource timebase: mask: 0xffffffffffffffff max_cycles: 0x8a60dd6a9, max_idle_ns: 440795204056 ns

clocksource: timebase mult[1aaaaaab] shift[24] registered

Console: colour dummy device 80x25

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 16384 (order: 5, 131072 bytes)

Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes)

e500 family performance monitor hardware support registered

Brought up 4 CPUs

devtmpfs: initialized

clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns

xor: measuring software checksum speed

   8regs     :  3187.000 MB/sec

   8regs_prefetch:  2606.000 MB/sec

   32regs    :  3187.000 MB/sec

   32regs_prefetch:  2740.000 MB/sec

xor: using function: 32regs (3187.000 MB/sec)

NET: Registered protocol family 16

Bman ver:0a02,02,01

qman-fqd addr 0x00000001fe800000 size 0x800000

qman-pfdr addr 0x00000001fc000000 size 0x2000000

Qman ver:0a01,03,01,03

Machine: fsl,T1040D4RDB

SoC family: QorIQ T1040

SoC ID: svr:0x85280011, Revision: 1.1

Found FSL PCI host bridge at 0x0000000ffe240000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe240000  ranges:

 MEM 0x0000000c00000000..0x0000000c0fffffff -> 0x00000000e0000000

  IO 0x0000000ff8000000..0x0000000ff800ffff -> 0x0000000000000000

/pcie@ffe240000: PCICSRBAR @ 0xff000000

setup_pci_atmu: end of DRAM 200000000

/pcie@ffe240000: Setup 64-bit PCI DMA window

/pcie@ffe240000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe240000: DMA window size is 0xe0000000

EDAC PCI0: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe240000.pcie (INTERRUPT)

MPC85xx_edac acquired irq 20 for PCI Err

MPC85xx_edac PCI err registered

Found FSL PCI host bridge at 0x0000000ffe250000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe250000  ranges:

 MEM 0x0000000c10000000..0x0000000c1fffffff -> 0x00000000e0000000

  IO 0x0000000ff8010000..0x0000000ff801ffff -> 0x0000000000000000

/pcie@ffe250000: PCICSRBAR @ 0xff000000

setup_pci_atmu: end of DRAM 200000000

/pcie@ffe250000: Setup 64-bit PCI DMA window

/pcie@ffe250000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe250000: DMA window size is 0xe0000000

EDAC PCI1: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe250000.pcie (INTERRUPT)

MPC85xx_edac acquired irq 21 for PCI Err

MPC85xx_edac PCI err registered

Found FSL PCI host bridge at 0x0000000ffe260000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe260000  ranges:

 MEM 0x0000000c20000000..0x0000000c2fffffff -> 0x00000000e0000000

  IO 0x0000000ff8020000..0x0000000ff802ffff -> 0x0000000000000000

/pcie@ffe260000: PCICSRBAR @ 0xff000000

setup_pci_atmu: end of DRAM 200000000

/pcie@ffe260000: Setup 64-bit PCI DMA window

/pcie@ffe260000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe260000: DMA window size is 0xe0000000

EDAC PCI2: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe260000.pcie (INTERRUPT)

MPC85xx_edac acquired irq 22 for PCI Err

MPC85xx_edac PCI err registered

Found FSL PCI host bridge at 0x0000000ffe270000. Firmware bus number: 0->0

PCI host bridge /pcie@ffe270000  ranges:

 MEM 0x0000000c30000000..0x0000000c3fffffff -> 0x00000000e0000000

  IO 0x0000000ff8030000..0x0000000ff803ffff -> 0x0000000000000000

/pcie@ffe270000: PCICSRBAR @ 0xff000000

setup_pci_atmu: end of DRAM 200000000

/pcie@ffe270000: Setup 64-bit PCI DMA window

/pcie@ffe270000: WARNING: Outbound window cfg leaves gaps in memory map. Adjusting the memory map could reduce unnecessary bounce buffering.

/pcie@ffe270000: DMA window size is 0xe0000000

EDAC PCI3: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err: DEV ffe270000.pcie (INTERRUPT)

MPC85xx_edac acquired irq 23 for PCI Err

MPC85xx_edac PCI err registered

software IO TLB [mem 0xfbfff000-0xfffff000] (64MB) mapped at [c0000000fbfff000-c0000000ffffefff]

PCI: Probing PCI hardware

fsl-pci ffe240000.pcie: PCI host bridge to bus 0000:00

pci_bus 0000:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x0000-0xffff])

pci_bus 0000:00: root bus resource [mem 0xc00000000-0xc0fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0000:00: root bus resource [bus 00]

pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0000:00:00.0: PCI bridge to [bus 01-ff]

fsl-pci ffe250000.pcie: PCI host bridge to bus 0001:00

pci_bus 0001:00: root bus resource [io  0x21000-0x30fff] (bus address [0x0000-0xffff])

pci_bus 0001:00: root bus resource [mem 0xc10000000-0xc1fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0001:00: root bus resource [bus 00]

pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0001:00:00.0: PCI bridge to [bus 01-ff]

fsl-pci ffe260000.pcie: PCI host bridge to bus 0002:00

pci_bus 0002:00: root bus resource [io  0x32000-0x41fff] (bus address [0x0000-0xffff])

pci_bus 0002:00: root bus resource [mem 0xc20000000-0xc2fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0002:00: root bus resource [bus 00]

pci 0002:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0002:00:00.0: PCI bridge to [bus 01-ff]

fsl-pci ffe270000.pcie: PCI host bridge to bus 0003:00

pci_bus 0003:00: root bus resource [io  0x43000-0x52fff] (bus address [0x0000-0xffff])

pci_bus 0003:00: root bus resource [mem 0xc30000000-0xc3fffffff] (bus address [0xe0000000-0xefffffff])

pci_bus 0003:00: root bus resource [bus 00]

pci 0003:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring

pci 0003:00:00.0: PCI bridge to [bus 01-ff]

PCI: Cannot allocate resource region 0 of device 0000:00:00.0, will remap

PCI: Cannot allocate resource region 0 of device 0001:00:00.0, will remap

PCI: Cannot allocate resource region 0 of device 0002:00:00.0, will remap

PCI: Cannot allocate resource region 0 of device 0003:00:00.0, will remap

pci 0000:00:00.0: BAR 0: no space for [mem size 0x01000000]

pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x01000000]

pci 0000:00:00.0: PCI bridge to [bus 01]

pci 0000:00:00.0:   bridge window [io  0x10000-0x1ffff]

pci 0000:00:00.0:   bridge window [mem 0xc00000000-0xc0fffffff]

pci_bus 0000:00: Some PCI device resources are unassigned, try booting with pci=realloc

pci 0001:00:00.0: BAR 0: no space for [mem size 0x01000000]

pci 0001:00:00.0: BAR 0: failed to assign [mem size 0x01000000]

pci 0001:00:00.0: PCI bridge to [bus 01]

pci 0001:00:00.0:   bridge window [io  0x21000-0x30fff]

pci 0001:00:00.0:   bridge window [mem 0xc10000000-0xc1fffffff]

pci_bus 0001:00: Some PCI device resources are unassigned, try booting with pci=realloc

pci 0002:00:00.0: BAR 0: no space for [mem size 0x01000000]

pci 0002:00:00.0: BAR 0: failed to assign [mem size 0x01000000]

pci 0002:00:00.0: PCI bridge to [bus 01]

pci 0002:00:00.0:   bridge window [io  0x32000-0x41fff]

pci 0002:00:00.0:   bridge window [mem 0xc20000000-0xc2fffffff]

pci_bus 0002:00: Some PCI device resources are unassigned, try booting with pci=realloc

pci 0003:00:00.0: BAR 0: no space for [mem size 0x01000000]

pci 0003:00:00.0: BAR 0: failed to assign [mem size 0x01000000]

pci 0003:00:00.0: PCI bridge to [bus 01]

pci 0003:00:00.0:   bridge window [io  0x43000-0x52fff]

pci 0003:00:00.0:   bridge window [mem 0xc30000000-0xc3fffffff]

pci_bus 0003:00: Some PCI device resources are unassigned, try booting with pci=realloc

raid6: int64x1  gen()   521 MB/s

raid6: int64x1  xor()   362 MB/s

raid6: int64x2  gen()   808 MB/s

raid6: int64x2  xor()   568 MB/s

raid6: int64x4  gen()  1177 MB/s

raid6: int64x4  xor()   724 MB/s

raid6: int64x8  gen()   982 MB/s

raid6: int64x8  xor()   654 MB/s

raid6: using algorithm int64x4 gen() 1177 MB/s

raid6: .... xor() 724 MB/s, rmw enabled

raid6: using intx1 recovery algorithm

vgaarb: loaded

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>

PTP clock support registered

EDAC MC: Ver: 3.0.0

bman-fbpr addr 0x00000001ff000000 size 0x1000000

Bman err interrupt handler present

Bman portal initialised, cpu 0

Bman portal initialised, cpu 1

Bman portal initialised, cpu 2

Bman portal initialised, cpu 3

Bman portals initialised

Qman err interrupt handler present

QMan: Allocated lookup table at 8000000000002000, entry count 131073

Qman portal initialised, cpu 0

Qman portal initialised, cpu 1

Qman portal initialised, cpu 2

Qman portal initialised, cpu 3

Qman portals initialised

Bman: BPID allocator includes range 32:32

Qman: FQID allocator includes range 256:512

Qman: FQID allocator includes range 32768:32768

Qman: CGRID allocator includes range 0:256

Qman: pool channel allocator includes range 1025:15

No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree

fsl-ifc ffe124000.localbus: Freescale Integrated Flash Controller

fsl-ifc ffe124000.localbus: IFC version 1.3, 8 banks

Switched to clocksource timebase

NET: Registered protocol family 2

TCP established hash table entries: 65536 (order: 7, 524288 bytes)

TCP bind hash table entries: 65536 (order: 8, 1048576 bytes)

TCP: Hash tables configured (established 65536 bind 65536)

UDP hash table entries: 4096 (order: 5, 131072 bytes)

UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 406748K (c000000003001000 - c00000001bd38000)

futex hash table entries: 1024 (order: 4, 65536 bytes)

HugeTLB registered 4 MB page size, pre-allocated 0 pages

HugeTLB registered 16 MB page size, pre-allocated 0 pages

HugeTLB registered 64 MB page size, pre-allocated 0 pages

HugeTLB registered 256 MB page size, pre-allocated 0 pages

HugeTLB registered 1 GB page size, pre-allocated 0 pages

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

ntfs: driver 2.1.32 [Flags: R/O].

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

async_tx: api initialized (async)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt

pcieport 0001:00:00.0: Signaling PME through PCIe PME interrupt

pcieport 0002:00:00.0: Signaling PME through PCIe PME interrupt

pcieport 0003:00:00.0: Signaling PME through PCIe PME interrupt

Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled

console [ttyS0] disabled

serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36, base_baud = 18750000) is a 16550A_FSL64

console [ttyS0] enabled

console [ttyS0] enabled

bootconsole [udbg0] disabled

bootconsole [udbg0] disabled

serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36, base_baud = 18750000) is a 16550A_FSL64

serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37, base_baud = 18750000) is a 16550A_FSL64

serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37, base_baud = 18750000) is a 16550A_FSL64

ePAPR hypervisor byte channel driver

brd: module loaded

loop: module loaded

st: Version 20101219, fixed bufsize 32768, s/g segs 256

fsl-sata ffe220000.sata: Sata FSL Platform/CSB Driver init

scsi host0: sata_fsl

ata1: SATA max UDMA/133 irq 68

fsl-sata ffe221000.sata: Sata FSL Platform/CSB Driver init

scsi host1: sata_fsl

ata2: SATA max UDMA/133 irq 69

fe8000000.nor: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00227e

Amd/Fujitsu Extended Query Table at 0x0040

  Amd/Fujitsu Extended Query version 1.3.

number of CFI chips: 1

nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xa3

nand: Micron MT29F8G08ABBCAH4

nand: 1024 MiB, SLC, erase size: 256 KiB, page size: 4096, OOB size: 224

nand: WARNING: fff800000.flash: the ECC used on your system is too weak compared to the one required by the NAND chip

Bad block table found at page 262080, version 0x01

Bad block table found at page 262016, version 0x01

fsl,ifc-nand fff800000.nand: IFC NAND device at 0xfff800000, bank 1

fsl_espi ffe110000.spi: cs=0, init_csmode=0x100008

fsl_espi ffe110000.spi: cs=1, init_csmode=0x100008

fsl_espi ffe110000.spi: cs=2, init_csmode=0x100008

m25p80 spi32766.0: n25q512ax3 (65536 Kbytes)

fsl_espi ffe110000.spi: at 0x8000080080952000 (irq = 53)

libphy: Fixed MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

libphy: Freescale XGMAC MDIO Bus: probed

Freescale FM module, FMD API version 21.1.0

Freescale FM Ports module

fsl_mac: fsl_mac: FSL FMan MAC API based driver

fsl_mac ffe4e0000.ethernet: FMan MEMAC

fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:05:d7:a1

fsl_mac ffe4e2000.ethernet: FMan MEMAC

fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:05:d7:a2

fsl_mac ffe4e4000.ethernet: FMan MEMAC

fsl_mac ffe4e4000.ethernet: FMan MAC address: 00:04:9f:05:d7:a3

fsl_mac ffe4e6000.ethernet: FMan MEMAC

fsl_mac ffe4e6000.ethernet: FMan MAC address: 00:04:9f:05:d7:a4

fsl_mac ffe4e8000.ethernet: FMan MEMAC

fsl_mac ffe4e8000.ethernet: FMan MAC address: 00:04:9f:05:d7:a5

fsl_dpa: FSL DPAA Ethernet driver

fsl_dpa: fsl_dpa: Probed interface eth0

fsl_dpa: fsl_dpa: Probed interface eth1

fsl_dpa: fsl_dpa: Probed interface eth2

fsl_dpa: fsl_dpa: Probed interface eth3

fsl_dpa: fsl_dpa: Probed interface eth4

fsl_advanced: FSL DPAA Advanced drivers:

fsl_proxy: FSL DPAA Proxy initialization driver

fsl_dpa_shared: FSL DPAA Shared Ethernet driver

fsl_dpa_macless: FSL DPAA MACless Ethernet driver

fsl_oh: FSL FMan Offline Parsing port driver

e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k

e1000e: Copyright(c) 1999 - 2014 Intel Corporation.

fsl-of-dma ffe100300.dma: dma channel dma-uio0-0 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-1 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-2 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-3 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-4 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-5 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-6 initialized

fsl-of-dma ffe100300.dma: dma channel dma-uio0-7 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-0 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-1 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-2 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-3 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-4 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-5 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-6 initialized

fsl-of-dma ffe101300.dma: dma channel dma-uio1-7 initialized

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-pci: EHCI PCI platform driver

/soc@ffe000000/usb@210000: Invalid 'dr_mode' property, fallback to host mode

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 45, io mem 0xffe211000

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

usbcore: registered new interface driver usb-storage

i2c /dev entries driver

mpc-i2c ffe118000.i2c: timeout 1000000 us

rtc-ds1307 0-0068: rtc core: registered ds1337 as rtc0

mpc-i2c ffe118100.i2c: timeout 1000000 us

mpc-i2c ffe119000.i2c: timeout 1000000 us

mpc-i2c ffe119100.i2c: timeout 1000000 us

i2c i2c-1: Added multiplexed i2c bus 4

i2c i2c-1: Added multiplexed i2c bus 5

i2c i2c-1: Added multiplexed i2c bus 6

i2c i2c-1: Added multiplexed i2c bus 7

ata1: No Device OR PHYRDY change,Hstatus = 0xa0000000

ata1: SATA link down (SStatus 10 SControl 300)

pca954x 1-0077: registered 4 multiplexed busses for I2C switch pca9546

ata2: No Device OR PHYRDY change,Hstatus = 0x80000000

ata2: SATA link down (SStatus 10 SControl 300)

md: raid6 personality registered for level 6

md: raid5 personality registered for level 5

md: raid4 personality registered for level 4

Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software

EDAC MC0: Giving out device to module MPC85xx_edac controller mpc85xx_mc_err: DEV mpc85xx_mc_err (INTERRUPT)

MPC85xx_edac acquired irq 490 for MC

MPC85xx_edac MC err registered

qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc@ffe000000/sdhc@114000: voltage-ranges unspecified

sdhci-esdhc ffe114000.sdhc: No vmmc regulator found

sdhci-esdhc ffe114000.sdhc: No vqmmc regulator found

mmc0: SDHCI controller on ffe114000.sdhc [ffe114000.sdhc] using ADMA 64-bit

platform caam_qi: Linux CAAM Queue I/F driver initialised

caam ffe300000.crypto: Instantiated RNG4 SH1

caam ffe300000.crypto: device ID = 0x0a12040000000000 (Era 6)

caam ffe300000.crypto: job rings = 4, qi = 1

caam algorithms registered in /proc/crypto

platform caam_qi: algorithms registered in /proc/crypto

caam_jr ffe301000.jr: registering rng-caam

caam ffe300000.crypto: fsl,sec-v5.0 algorithms registered in /proc/crypto

Freescale USDPAA process driver

fsl-usdpaa: no region found

Freescale USDPAA process IRQ driver

fsl-pme ffe316000.pme: ver: 0x00100202

Freescale pme2 db driver

Freescale pme2 scan driver

fsl-pme2-scan: device pme_scan registered

Freescale hypervisor management driver

fsl-hv: no hypervisor found

ipip: IPv4 over IPv4 tunneling driver

Initializing XFRM netlink socket

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

NET: Registered protocol family 15

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

fsl_generic: FSL DPAA Generic Ethernet driver

rtc-ds1307 0-0068: setting system clock to 2018-05-25 11:01:30 UTC (1527246090)

md: Waiting for all devices to be available before autodetect

md: If you don't use raid, use raid=noautodetect

md: Autodetecting RAID arrays.

md: Scanned 0 and added 0 devices.

md: autorun ...

md: ... autorun DONE.

RAMDISK: gzip image found at block 0

VFS: Mounted root (ext2 filesystem) on device 1:0.

devtmpfs: mounted

Freeing unused kernel memory: 388K (c000000000b73000 - c000000000bd4000)

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 75970

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 75970

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 77050

INIT: version 2.88 booting

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 75970

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 75970

INIT: No inittab file found

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 77050

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 77050

 

Enter runlevel: 5

INIT: Entering runlevel: 5

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 77050

EXT2-fs (ram0): error: ext2_lookup: deleted inode referenced: 77050

INIT: no more processes left in this runlevel

0 项奖励
回复
2 回复数

2,353 次查看
yipingwang
NXP TechSupport
NXP TechSupport

The fsl-image-full image is too large, it is not suitable to boot from ramdisk, you could deploy full rootfs image to SD/USB/SATA, then boot rootfs from SD/USB/SATA. 

You could use fsl-image-core image to do ramdisk boot.

Please refer to the following procedure to deploy rootfs to boot Kernel and filesystem from SD/MMC.

1. Use the mkfs.ext2 command to create the filesystems.

# mkfs.ext2 /dev/sdb2

2. Copy the file system to SD card by extracting the QorIQ_SDK_V1.6_ROOTFS_Image.tar.gz from rebuild image ISO, remove the tarball after extracting rootfs.

# cp QorIQ_SDK_V1.6_ROOTFS_Image.tar.gz .

# tar -zxvf QorIQ_SDK_V1.6_ROOTFS_Image.tar.gz

# rm QorIQ_SDK_V1.6_ROOTFS_Image.tar.gz

3. Plug in the SD card to the target board and power on.

4. Set the environment in uboot for SD boot.

# setenv bootfile uImage

# setenv fdtfile uImage.dtb

# setenv bootcmd 'setenv bootargs root=/dev/mmcblk0p2 rw rootdelay=5 console=$consoledev,$baudrate;mmcinfo;ext2load mmc 0:2 $loadaddr /boot/$bootfile;ext2load mmc 0:2 $fdtaddr /boot/$fdtfile;bootm $loadaddr - $fdtaddr'

# boot

0 项奖励
回复

2,338 次查看
WmBAnderson
Contributor I
1) Is there something special about V1.6 or is it just for illustration? 2) V1.6 @ https://freescaleesd.flexnetoperations.com/337170/171/8531171/QorIQ%20SDK%20v1.6%20PPCE6500%20Image.... does not respond to a download request. Has it been removed? 3) In your instructions below the boot does not find my uImage...bin does it need the link or the bin file itself? R/ Bill
0 项奖励
回复