sdk2.0 fsl-toolchain building in fedora

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sdk2.0 fsl-toolchain building in fedora

1,068件の閲覧回数
vidyasagartata
Contributor II

Dear All,

Unable to build fsl-toolchain from  QorQSDK 2.0. The build gets stuck at 69%.

 

Building fsl-toolchain fails.The build gets stuck at 69% and doesn’t show any errors. Following steps followed for building the image

< ![if !supportLists]>1.       Install QoRIQ_Linux_SDK_v2.0-AARCH_Yocto_cache.iso< /span>

  1. Install QoRIQ_Linux_SDK_v2.0-SOURCE.iso
  2. Setup Host environment ( ! Fedora 22) by installing following packages
  3. gaw k make wget tar bzip2 gzip python unzip perl patch \
  4. diffutils diffstat git cpp gcc gcc-c++ glibc-devel texinfo chrpath \
  5. ccache perl-Data-Dumper perl-Text-ParseWords perl-Thread-Queue socat \
  6. findutils which SDL-devel xterm
  7. . ./fsl-setup-env –m t2080rdb –t 4 –j4
  8. bitbake fsl-toolchain

I am able to build “fsl-image-minimal”  target but unable to build fsl-toolchain.

Thanks,

Vidya

0 件の賞賛
返信
2 返答(返信)

830件の閲覧回数
vidyasagartata
Contributor II

Thanks our problem has resolved.

0 件の賞賛
返信

830件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please execute the script "sources/meta-freescale/scripts/host-prepare.sh" before step 8.

Please provide the console log if your problem remains.

Thanks,

Yiping

0 件の賞賛
返信