issue in using #pragma omp simd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

issue in using #pragma omp simd

1,215件の閲覧回数
mohamedhusain
Contributor I

Not getting altivec instructions on compiling the following code

testsimd.cpp

////////////////////////////////////////

#include <omp.h>

int main()
{
    int LEN=3200;
    int __attribute__ ((aligned(16))) a[LEN], b[LEN], c[LEN];
#pragma omp simd safelen(16) aligned(a:16) aligned(b:16) aligned(c:16)
    for( int i=0; i<LEN; i++ )
       a[i] = a[i]*b[i];

    return 0;
}

///////////////

compiled using

 $CXX -S testsimd.cpp -fopenmp -fopenmp-simd -maltivec -mabi=altivec -I /opt/fsl-qoriq/2.0/sysroots/ppc64e6500-fsl-linux/usr/lib64/gcc/powerpc64-fsl-linux/4.9.2/include/

echo $CXX
powerpc64-fsl-linux-g++ -mhard-float -m64 -mcpu=e6500 --sysroot=/opt/fsl-qoriq/2.0/sysroots/ppc64e6500-fsl-linux

$CXX -v
Using built-in specs.
COLLECT_GCC=powerpc64-fsl-linux-g++
COLLECT_LTO_WRAPPER=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/libexec/powerpc64-fsl-linux/gcc/powerpc64-fsl-linux/4.9.2/lto-wrapper
Target: powerpc64-fsl-linux
Configured with: /home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/work-shared/gcc-4.9.2-r0/gcc-4.9.2/configure --build=x86_64-linux --host=x86_64-fslsdk-linux --target=powerpc64-fsl-linux --prefix=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr --exec_prefix=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr --bindir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/bin/powerpc64-fsl-linux --sbindir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/bin/powerpc64-fsl-linux --libexecdir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/libexec/powerpc64-fsl-linux --datadir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/share --sysconfdir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/etc --sharedstatedir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/com --localstatedir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/var --libdir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/lib/powerpc64-fsl-linux --includedir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/include --oldincludedir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/include --infodir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/share/info --mandir=/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr/share/man --disable-silent-rules --disable-dependency-tracking --with-libtool-sysroot=/home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/sysroots/x86_64-nativesdk-fslsdk-linux --with-gnu-ld --enable-shared --enable-languages=c,c++ --enable-threads=posix --enable-multilib --enable-c99 --enable-long-long --enable-symvers=gnu --enable-libstdcxx-pch --program-prefix=powerpc64-fsl-linux- --without-local-prefix --enable-target-optspace --enable-lto --enable-libssp --disable-bootstrap --disable-libmudflap --with-system-zlib --with-linker-hash-style=gnu --enable-linker-build-id --with-ppl=no --enable-checking=release --enable-cheaders=c_global --with-gxx-include-dir=/not/exist/usr/include/c++/4.9.2 --with-build-time-tools=/home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/sysroots/x86_64-linux/usr/powerpc64-fsl-linux/bin --with-sysroot=/not/exist --with-build-sysroot=/home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/sysroots/b4860qds-64b --with-long-double-128 --enable-poison-system-directories --with-mpfr=/home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/sysroots/x86_64-nativesdk-fslsdk-linux --with-mpc=/home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/sysroots/x86_64-nativesdk-fslsdk-linux --enable-nls --enable-__cxa_atexit --with-isl=/home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/sysroots/x86_64-nativesdk-fslsdk-linux/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr --with-cloog=/home/jenkins/ci/iso-make/master/b4860qds-64b/build_b4860qds-64b/tmp/sysroots/x86_64-nativesdk-fslsdk-linux/opt/fsl-qoriq/2.0/sysroots/x86_64-fslsdk-linux/usr
Thread model: posix
gcc version 4.9.2 (GCC)

testsimd.s

//////////////////////////

...

li 10,0
stw 10,48(31)
b .L2
.L3:
ld 8,64(31)
lwz 10,48(31)
extsw 10,10
sldi 10,10,2
add 10,8,10
lwz 10,0(10)
extsw 8,10
ld 7,80(31)
lwz 10,48(31)
extsw 10,10
sldi 10,10,2
add 10,7,10
lwz 10,0(10)
extsw 10,10
mullw 10,8,10
extsw 8,10
ld 7,64(31)
lwz 10,48(31)
extsw 10,10
sldi 10,10,2
add 10,7,10
stw 8,0(10)
lwz 10,48(31)
addi 10,10,1
stw 10,48(31)
.L2:
lwz 10,48(31)
cmpw 7,10,9
blt 7,.L3
li 10,0

0 件の賞賛
返信
1 返信

1,088件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please create the program as the following.

$ cat test_altivec.c
#include
int main()
{
int LEN=3200;
float __attribute__ ((aligned(16))) a[LEN], b[LEN], c[LEN];
*(vector float*)c = (*(vector float*)a)*(*(vector float*)b);
return 0;
}

Build the program with the following command

$ source /opt/fsl-qoriq/2.0/environment-setup-ppc64e6500-fsl-linux

$ ${CC} test_altivec.c -maltivec -mabi=altivec -o test_altivec

$ powerpc64-fsl-linux-objdump -S test_altivec >test_altivec.s

You will find part of the disassembly code as the following.

   10000700:   f9 3f 00 60     std     r9,96(r31)

   10000704:   e9 3f 00 60     ld     r9,96(r31)

   10000708:   e9 5f 00 40     ld     r10,64(r31)

   1000070c:   7d a0 50 ce     lvx     v13,0,r10

   10000710:   e9 5f 00 50     ld     r10,80(r31)

   10000714:   7c 20 50 ce     lvx     v1,0,r10

   10000718:   10 1f 03 8c     vspltisw v0,-1

   1000071c:   10 00 01 84     vslw   v0,v0,v0

   10000720:   10 0d 00 6e     vmaddfp v0,v13,v1,v0

   10000724:   7c 00 49 ce     stvx   v0,0,r9


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信