Why is classifier_demo not supported on T1040 platform?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is classifier_demo not supported on T1040 platform?

1,323 Views
jakubhorak
Contributor I


The QorIQ SDK 1.9 manual mentions that the classifier_demo is not available for T1040. I tried to run that demo (with altered Fman RX port/Offline port configuration), but it doesn't work ("fragmentation_demo: Failed to execute the FMC Model"). Is there a hardware restriction for why it shouldn't work?

Labels (1)
0 Kudos
Reply
2 Replies

1,185 Views
Pavel
NXP Employee
NXP Employee

There is no information for restriction for the classifier_demo on the T1040 board. Look at the following pages:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-B036AE9A-3E5B-4B2D-88...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-EBA4AB66-B817-405A-AA...

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-90FEC516-749E-4C3A-A5...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,185 Views
jakubhorak
Contributor I

If you look at the first link

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-B036AE9A-3E5B-4B2D-88...

It says, and I quote:

Classifier_demo application supports the following platforms:

  • P2041
  • P4080
  • B4860
  • B4420
  • T4240
  • T2080

Nowhere it mentions T1040. The SDK doesn't contain config files for classifier demo for T1040.

This quote together with the fact that it _doesn't_ work suggest that it is not supported. My question is: what's the reason for it not being supported and how can I fix it.

Best regards,

Jakub Horak

0 Kudos
Reply