What is RAMDISK, RCW and FMan Microcode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is RAMDISK, RCW and FMan Microcode

ソリューションへジャンプ
5,934件の閲覧回数
yusufalti333
Contributor IV

Hi nxp community,

I am new in embedded world and these terms. Trying to figure out everything I read in documentation https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf and apply everything I learn to my T1042D4RDB-64b using Yocto and U-boot. I searched google to learn what those terms mean but couldn't figure out. Is there anyone who can clearly tell me what does RAMDISK,RCW and FMan Microcode do/mean.

ラベル(1)
0 件の賞賛
返信
1 解決策
5,734件の閲覧回数
ufedor
NXP Employee
NXP Employee

RCW (Reset Configuration Word):

The chip uses an external memory interface to import a subset of the reset configuration information from a memory device during reset. Such information is called reset configuration word (RCW) data.

Detailed description is provided in the QorIQ T1040 Reference Manual, 4.6.5 Reset configuration word (RCW)

FMan (Frame Manager) microcode:

Description of the FMan functions which require microcode is provided in the T1040 QorIQ Data Path Acceleration Architecture (DPAA) Reference Manual, 5.13 Frame Manager—FMan Controller.

RAMDISK:

Software RAM disk is the normal RAM in main memory as if it were a partition on a hard drive rather than actually accessing the data bus normally used for secondary storage such as hard disk. Additional details can be found on Linux forums.

NXP Linux SDK contains all necessary tools for RAM disk image preparation and deployment - refer to the SDK Documentation:

Submit Form 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,735件の閲覧回数
ufedor
NXP Employee
NXP Employee

RCW (Reset Configuration Word):

The chip uses an external memory interface to import a subset of the reset configuration information from a memory device during reset. Such information is called reset configuration word (RCW) data.

Detailed description is provided in the QorIQ T1040 Reference Manual, 4.6.5 Reset configuration word (RCW)

FMan (Frame Manager) microcode:

Description of the FMan functions which require microcode is provided in the T1040 QorIQ Data Path Acceleration Architecture (DPAA) Reference Manual, 5.13 Frame Manager—FMan Controller.

RAMDISK:

Software RAM disk is the normal RAM in main memory as if it were a partition on a hard drive rather than actually accessing the data bus normally used for secondary storage such as hard disk. Additional details can be found on Linux forums.

NXP Linux SDK contains all necessary tools for RAM disk image preparation and deployment - refer to the SDK Documentation:

Submit Form 

0 件の賞賛
返信
5,643件の閲覧回数
WmBAnderson
Contributor I
ufedor, Is there a cross reference that shows which version of the QorIQ Linux SDK will build the corect software load for the particular version of T1040 I have? I've built SDK 1.7 & 1.8 niether of which has the fsl_fman_ucode_t1040_r1.1_106_4_18.bin I believe I need for my board. My U-Boot indicates I have Fman1 microcode version 106.4.18 running on a T1040E Version 1.1 Regards, Bill
0 件の賞賛
返信