Uboot sequence boot in T2080RDB with NOR Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot sequence boot in T2080RDB with NOR Flash

3,749 Views
alouizied
Contributor I

Hi everyone,

I work with the Qoriq T2080RDB Board, i don't have the Codewarrior Tap for debugging (I expected to be delivered) and neither the CodeWarrior development suite.

I just want to understand the boot sequence of Uboot in the Qoriq T2080rdb with the NOR Flash and the addressing mode (Physical or virtual address).

Her we have the Flash memory Map of Qoriq T2080RDB Board   :

128M NOR Flash memory Map

-------------------------

Start Address End Address Definition Max size

0xEFF40000 0xEFFFFFFF u-boot (current bank) 768KB

0xEFF20000 0xEFF3FFFF u-boot env (current bank) 128KB

0xEFF00000 0xEFF1FFFF FMAN Ucode (current bank) 128KB

0xEFE00000 0xEFE3FFFF PHY CS4315 firmware 256KB

0xED300000 0xEFEFFFFF rootfs (alt bank) 44MB

0xEC800000 0xEC8FFFFF Hardware device tree (alt bank) 1MB

0xEC020000 0xEC7FFFFF Linux.uImage (alt bank) 7MB + 875KB

0xEC000000 0xEC01FFFF RCW (alt bank) 128KB

0xEBF40000 0xEBFFFFFF u-boot (alt bank) 768KB

0xEBF20000 0xEBF3FFFF u-boot env (alt bank) 128KB

0xEBF00000 0xEBF1FFFF FMAN ucode (alt bank) 128KB

0xEBE00000 0xEBE3FFFF PHY CS4315 firmware (alt bank) 256KB

0xE9300000 0xEBEFFFFF rootfs (current bank) 44MB

0xE8800000 0xE88FFFFF Hardware device tree (cur bank) 1MB

0xE8020000 0xE86FFFFF Linux.uImage (current bank) 7MB + 875KB

0xE8000000 0xE801FFFF RCW (current bank) 128KB

We can see that U-boot is mapped at 0xEFF40000-0xEFFFFFFF and 0xEBF40000-0xEBFFFFFF in the NOR Flash memory. Why do we have 2 versions of uboot "current bank" and "alternative bank"?

According to the datasheet of the Processor E6500, at the power-up the CPU0 begin to execute his first instruction at the address 0xFFFF_FFFC that correspond at the Reset address.

But in Uboot the Reset vector is mapped at 0xEFFF_FFFC and not at 0xFFFF_FFFC, why is that? Do we use Physical address or Virtual address?

According to the dissembler code of U-boot, after the reset vector at 0xEFFF_FFFC, Uboot jump at the address 0xEFFF_0000 that correspond to the entry point "_start_e500" where he clear some register, setup the interrupt vector table, etc. After he finish the initialisation phase, U-boot jump to the address 0xEFF40000.

I want to know where the code of U-boot is executed in the NOR flash memory or in the DDR3 SDRAM memory?

When i use the command "md 0x00000100" in U-boot, do we visualise the NOR Flash memory or the DDR3 SDRAM memory? It's physical or Virtual address that we visualise?

When i use the command "bdinfo" in U-boot i have:

=> bdinfo

memstart    = 0x00000000

memsize     = 0x100000000

flashstart  = 0xE8000000

flashsize   = 0x08000000

flashoffset = 0x00000000

sramstart   = 0x00000000

sramsize    = 0x00000000

immr_base   = 0xFE000000

bootflags   = 0x00000000

intfreq     = 1799.820 MHz

busfreq     = 599.940 MHz

addressing  = 36-bit

ethaddr     = 00:0D:DD:DD:DD:DD

IP addr     = 192.168.1.3

baudrate    = 115200 bps

relocaddr   = 0x7FEF0000

In " addressing" we have 36 bits, this corresponds to what?

Does u-boot relocate himself at the address 0x7FEF0000? if yes, for what purpose?

Best Regards

Zied

Labels (1)
Tags (1)
0 Kudos
Reply
6 Replies

2,420 Views
ufedor
NXP Employee
NXP Employee

> Why do we have 2 versions of uboot "current bank" and "alternative bank"?

It is recommended to program new/test versions of U-Boot and other images to "alternative bank" so the board could be boot from "current bank" if something went wrong with the "alternative bank". In hardware the NOR FLASH memory is divided into eight memory banks with 16MB size each by means of CPLD controlling three NOR Flash address lines (A23, A24, A25). In software only two banks (halves) are used by alternating A25 address line.

How does Processor jump to start address of U-Boot?

Please note that after reset the IFC_CSPR0[V]=1 and IFC_AMASK0[AM]=0 (Memory Bank Size 4GB) – i.e. in case of the T2080RDB NOR boot the whole address space (4GB) will "contain" 128MB "copies" of the NOR Flash and the last (upper) word of the NOR Flash will appear as the last word of the 4GB address space (0xFFFF_FFFC).

Also please consider that:

1) MMU has one 4-Kbyte page defined at 0x0_FFFF_Fnnn – refer to the QorIQ T2080 Family Reference Manual, 4.3.3 Boot Space Translation.

2) the core begins execution with the instruction at effective address 0x0_FFFF_FFFC.

0 Kudos
Reply

2,420 Views
sandratrujillog
Contributor III

About this I have a question, If I want to program a version of U-boot to "alternative bank" I need to use the following commands to flash a new U-boot:

=>tftp 1000000 <u-boot_file_name>.bin 
=>protect off <u-boot_start_addr> +$filesize 
=>erase <u-boot_start_addr> +$filesize 
=>cp.b 1000000 <u-boot_start_addr> $filesize 
=>protect on <u-boot_start_addr> +$filesize 
=>cpld reset altbank

How can I find the u-boot_start_addr and the filesize? What is the value of u-boot_start_addr that I need?

0 Kudos
Reply

2,420 Views
ufedor
NXP Employee
NXP Employee

Please refer to the SDK Documentation:

Submit Form 

The "$filesize" is a variable which is assigned its value after the TFTP transfer.

0 Kudos
Reply

2,420 Views
sandratrujillog
Contributor III

Do I have to use the range start of U-boot (alternative bank)? Specifically 0xebf40000?

0 Kudos
Reply

2,420 Views
ufedor
NXP Employee
NXP Employee

> Do I have to use the range start of U-boot (alternative bank)? Specifically 0xebf40000?

The question is not fully clear.

0 Kudos
Reply

2,420 Views
ufedor
NXP Employee
NXP Employee

> if the value I need for u-boot_start_addr is 0xebf40000

In the NOR flash memory map table it is written:

Range StartRange EndDefinitionSize
0xebf40000
0xebffffff
U-Boot (alternate bank)768 KB
0 Kudos
Reply