The problem with writing IFC SRAM in U-Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The problem with writing IFC SRAM in U-Boot

905 Views
mertsalar137
Contributor I

Hi,

I am encountering an issue with writing to the IFC SRAM (0xff800000 address) in U-boot on our custom board with a T2080 processor. I have successfully developed a baremetal IFC NAND flash driver that works correctly. However, when integrating this driver into U-boot, I am unable to write to the IFC SRAM address. Strangely, in the baremetal environment, I do not encounter any problems with writing to this address. I have attempted to use the "mw" command in U-boot, but it does not seem to have any effect. Could you help me pls?

0 Kudos
Reply
1 Reply

830 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hope this post finds you well,

Please note that an appropriate API is required.

I would like to inform you that our U-boot contains the necessary APIs for the appropriate operation of the device.

For more information for this process I highly recommend you to check the following link:

https://u-boot.readthedocs.io/en/latest/api/dm.html

Best Regards,

Hector Villarruel

0 Kudos
Reply