T4240rdb network performance issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240rdb network performance issue

1,912件の閲覧回数
sedat_altun
Contributor III

Hi everybody,

I got inconsistent ipsec null performance results while  using t4240rdb board with dpaa ports fman1 and fman2. I have two t4240rdb boards using kernel, dtb, filesystem taken from sdk 1.6.

I use ixia  to  generate packets. While I am sending packets at a rate of % 100 only in one direction the performance is 400mbps.But while I inject packets at a rate of % 100 in both direction i got 300mbps as an aggregate performance. Why the aggregate performance is not around 2×400 mbps on such a high performance board. I couldnt even reach 400mbps.

After conducting some tests I reached  an  interesting result. If I decrease the traffic rate near % 60 I got an aggregate 2×420 mbps performance. And   I  observed the performance is starting to decrease if the packet drops started. I couldn't explain why the performance is dramatically decreasing if I exceed a traffic rate % 60. As if there is a rate control mechanism which limits the total packet throughput. Any help will be appreciated.

Best regards

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,748件の閲覧回数
bpe
NXP Employee
NXP Employee

There must be something not configured properly. Suggestions:

1. Use the most recent SDK

2. Follow the recommendations at the link below:

https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK_1.9/GUID-15BE1669-CD22-45D9-B7...

Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,748件の閲覧回数
sedat_altun
Contributor III

Thank you for your response,

I also tried most recent SDK but nothing changed.

It maybe due to traffic shaping or policing configuration of the t4240.