T4240rdb login error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240rdb login error

2,102 Views
varunkjayan
Contributor II

hi

i have loaded an image created ext2 file using tftp server and the booting is done on

1000000 4000000 c00000 respectively and  when the image gets loaded it is asking for password

ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQCAbRFZB/d+dNLX5xwioHzpSaKzrYIfpMqubs1FXeAhOndTWb0SWBEzni4gPon47IC5VI8YBVzQB91L4sM8ErwD+y1RhKFrki/SZ4rr0N8lWOE+P0

Fingerprint: md5 06:28:63:d6:9a:d4:22:14:e3:70:66:0b:1f:29:23:aa

dropbear.

Starting Distributed Compiler Daemon: distcc.

Starting network benchmark server: netserver.

Starting system log daemon...0

Starting kernel log daemon...0

Starting internet superserver: xinetd.

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon

   ...done.

Stopping Bootlog daemon: bootlogd.

Poky (Yocto Project Reference Distro) 1.6.1 :::::eth0 /dev/ttyS0

:::::eth0 login: root

Password:

Login incorrect

please reply

Labels (1)
0 Kudos
Reply
2 Replies

1,939 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello varun k jayan,

Probably there is problem with the rootfs filesystem, would you please attach the whole kernel booting log(also including the tftp download information)?

Please refer to the following normal boot log

Public key portion is:

ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQC6/U51C3rCdf5NUfaE5CYQoVb4v/zvPjphM0MPAcSeIqMMXT0julUyBB0on8+C+6vY6ZIn9YBakj4ICtOlg7h6j0LFdfA1/AyJbeefMPFSz+zohI2285jpYtOn6s7xDptX7QM15BN1H+cSsL/pTL9pxX2BPw6iW/t23BDo7PnwIY+CUlGP6bVAvY1NK84utczw8bCZZO20deak4yAGcrFEg/wW5fSEHkkwX4wwMOFv6RVZLgPPPshQMIx92fz+LU32DEhD77j+UZouDjw3RVgW3ipOcGhCV2wmPZchUKdWe8BKM34yyoiWu8+6QNgxAuyWYfLg06JgRNaHBBqsCS2B root@t4240qds

Fingerprint: md5 5f:0a:09:5b:4e:af:20:10:04:17:3b:ab:cb:b4:2e:e2

dropbear.

Starting network benchmark server: netserver.

Starting system log daemon...0

Starting kernel log daemon...0

Starting internet superserver: xinetd.

Stopping Bootlog daemon: bootlogd.

Poky (Yocto Project Reference Distro) 1.6.1 t4240qds /dev/ttyS0

t4240qds login: root

root@t4240qds:~#


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,939 Views
varunkjayan
Contributor II

i used

tftp 1000000 uImage

tftp 4000000 fsl-imag-core-t4240rdb.ext2.gz.u-boot

tftp c00000  uImage-t4240rdb-usdpaa.dtb

since tftp 2000000 does not hold more than 44mb , My image is around 73.5 mb

0 Kudos
Reply