T4240 data rate ratios

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240 data rate ratios

3,161 Views
davidcchung
NXP Employee
NXP Employee

Why can I not set all the DDR data rate ratios that the reference manual says are supported by the RCW “MEM_PLL_RAT” field bits 10-15?

Labels (1)
Tags (4)
0 Kudos
Reply
2 Replies

2,957 Views
Saul_Salazar
NXP Employee
NXP Employee

There is a footnote in the T4240 reference manual that states “Not all ratios are supported due to frequency restrictions. Refer to the hardware specifications for the supported frequencies."


Hope it helps

0 Kudos
Reply

2,957 Views
addiyi
NXP Employee
NXP Employee

Do you try to use QCVS? Or what is your scenario?

Adrian

0 Kudos
Reply