T2080RDB: bootrom boot problem from NAND Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080RDB: bootrom boot problem from NAND Flash

2,927件の閲覧回数
flabyjacob
Contributor III

Hi,

Can somebody help me to program bootrom.bin in NAND Flash of T2080RDB EVM.

Note: I am able to program and boot bootrom.bin from the  alternate bank of NOR Flash of T2080RDB EVM as explained in the target.ref file provided in the t2080rdb bsp.

I have the following doubts too,

  • Does the bootrom not require rcw before it boot?
  • Do I need to change something in the bsp before building as it needs to boot from NAND Flash

Thanks & Regards

Flaby

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,520件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which OS and BSP is in question?

0 件の賞賛
返信

2,520件の閲覧回数
flabyjacob
Contributor III

Hi Fedor,

Thank you...

OS is vxWorks

BSP is fsl_t2080_rdb

Regards

Flaby

0 件の賞賛
返信

2,520件の閲覧回数
ufedor
NXP Employee
NXP Employee

Sorry, we do not support VxWorks BSP - please contact Wind River technical support.

0 件の賞賛
返信

2,520件の閲覧回数
flabyjacob
Contributor III

Thanks Fedor...
I will try the same...

Regards

Flaby

0 件の賞賛
返信