T2080RDB Simulator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,998件の閲覧回数
Faizanbaig
Contributor IV

Hi,

I am trying to work with T2080RDB. I want to know whether there is any Simulator that can help us in simulation and knowing the output like register view,memory dumps, UART messages before running the code on T2080 board.?

Any Suggestions would be appreciated.

 

Thanks,

Faizan

 

0 件の賞賛
返信
1 解決策
1,991件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior Development Studio for Power Architecture® Processors supports the following simulator models:
• B4xxx ISS simulators: Functional, unified simulator based on SC3900 core ISS simulator and PA e6500 JIT-ISS simulator. Currently, B4860iss and B4420iss simulator models are supported.

• T4xxx ISS simulators: Functional simulator based on PA e6500 JIT-ISS simulator.
Currently, T4240iss simulator model is supported, but only for Linux64 systems.

You could download and install CodeWarrior for PA 10.5.1 from the following link.

https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing

After install CodeWarrior, please refer to C:\Freescale\CW_PA_v10.5.1\PA\Help\PDF\PA Simulator User Guide.pdf and section "5.3.1 CCSSIM2 ISS" in Targeting_PA_Processors.pdf for details.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,992件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior Development Studio for Power Architecture® Processors supports the following simulator models:
• B4xxx ISS simulators: Functional, unified simulator based on SC3900 core ISS simulator and PA e6500 JIT-ISS simulator. Currently, B4860iss and B4420iss simulator models are supported.

• T4xxx ISS simulators: Functional simulator based on PA e6500 JIT-ISS simulator.
Currently, T4240iss simulator model is supported, but only for Linux64 systems.

You could download and install CodeWarrior for PA 10.5.1 from the following link.

https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing

After install CodeWarrior, please refer to C:\Freescale\CW_PA_v10.5.1\PA\Help\PDF\PA Simulator User Guide.pdf and section "5.3.1 CCSSIM2 ISS" in Targeting_PA_Processors.pdf for details.

0 件の賞賛
返信