T2080QDS Memory may not work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080QDS Memory may not work

1,921 次查看
crashbuzz
Contributor I

Hello NXP community,

I have powered my T2080 QDS board as usual and suddenly the U-Boot output was like in the screenshot below. Can anyone provide me with a solution on how to get rid of this error? Currently I am stuck at this point not knowing how to move on.

u-boot.JPG

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

1,744 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello crashbuzz,

First please make sure that you are using the original DDR provided in T2080QDS.

Please use the default clock(Core/Platform/DDR = 1800MHz/600MHz/1866MT/s) configuration on the target board.

Please configure your target board to the default switch settings.

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,744 次查看
crashbuzz
Contributor I

Hello yipingwang‌

thank you for the answer. Can you tell me which one is the "original DDR provided in T2080QDS". Maybe I have the wrong one.

Regards

0 项奖励
回复