T2080 VID question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 VID question

1,028 Views
xiaopengma
Contributor I

I have reviewed T4240 Data Sheet and T2080 Data Sheet,found that they may be woking on the same VID mechanism.

There is a Note in T4240 Data Sheet:

"9. If VID is known at initial start-up, set VDD=VID else if VID is not known at initial start-up, set VDD to 1.025V and change it

immediately, to VDD=VID after reading VID at the beginning of booting."

Does this Note apply to T2080?

Labels (1)
0 Kudos
Reply
1 Reply

924 Views
ufedor
NXP Employee
NXP Employee

Yes.

The same functioning is described in the T2080 QorIQ Integrated Multicore Communications Processor data sheet, 4.2.1 Voltage ID (VID) controllable supply.

0 Kudos
Reply