T2080 VCORE controller alternative?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 VCORE controller alternative?

3,055件の閲覧回数
davef
Contributor I

The 2-phase buck controller (IR36021) recommended for the T2080 core voltage supply (and implemented in the RDB) is obsolete.

Does NXP have a recommendation for a replacement controller that supports a manual VID programming facility (I2C or PMBUS)?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,905件の閲覧回数
abhijit_pethkar
Contributor II

Use LTM4676A from Linear Technology. We have used it in our design with T2081 Processor.

0 件の賞賛
返信

2,905件の閲覧回数
aneeshk
Contributor I

Hi,

Is there any suggestion for TI power controller module with external switch?

0 件の賞賛
返信

2,905件の閲覧回数
Pavel
NXP Employee
NXP Employee

There are no recommendations for replacing IR36021.

Use as Layerscape communications processor board schematic.

For example see the LS1088ARDB schematic:

https://www.nxp.com/downloads/en/printed-circuit-boards/LS1088ARDB-PB-DF.zip

 

This board uses the LTC3882 as buck converter.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信