T2080 USB control signals

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 USB control signals

859 次查看
paulagarcía-mor
Contributor I

If I don't use the USB power fault and usb power enable signals, would I have any problem with this interface?

I don't want to use them since I am using the same 5V regulator to supply USB and other devices, so I don't want USB controller to controls also those other devices.

Should I use a specific 5V source to USB so I can control it with the above mentioned signals or it is not necessary?

Thanks in advance.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

785 次查看
ufedor
NXP Employee
NXP Employee

It is possible to not use the signals in question, but the board designer still has to take precautions to eliminate possible hardware damage in case of USB device power failure.

0 项奖励
回复