T2080 SnVDD Power Requirement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 SnVDD Power Requirement

1,697件の閲覧回数
davef
Contributor I

1. Tables 6&7 of the T2080 datasheet specify SnVDD of 1.0W for all clocking scenarios. Does this figure refer to S1VDD & S2VDD combined, or 1.0W for S1VDD and 1.0W for S2VDD?

2. The T2080RDB card uses a 1A linear regulator for combined S1VDD & S2VDD. This seems borderline if one assumes the lesser 1.0W total power requirement. Is the 1.0W figure an absolute worst case maximum, or is the T2080RDB implementation perhaps lacking in terms of design margin?

ラベル(1)
0 件の賞賛
返信
1 返信

1,617件の閲覧回数
Bulat
NXP Employee
NXP Employee

1W is the maximum S1VDD+S2VDD power consumption, 1A current is enough. You can use other power source circuitry than used in the refrence design if you wish.

Regards,

Bulat

0 件の賞賛
返信