T2080 SerDes Register Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 SerDes Register Problem

1,323 次查看
xiaopengma
Contributor I

I noticed that some SerDes Register bit fields are set by RCW configuration and some are not.

For example SerDesx_LNnGCR0[PROTS] is not set by RCW configuration

and SerDesx_LNnGCR0[IF20BIT_EN] is set by RCW configuration.

This makes me confused.

If the PBL is complete with the right SerDes RCW configuration,

in my situation,SRDS_PRTCL_S1 = 0x6C SRDS_PRTCL_S2 = 0x2D,

should I need modify some SerDes Register bit fields manually?

标签 (1)
0 项奖励
回复
1 回复

1,184 次查看
ufedor
NXP Employee
NXP Employee

> should I need modify some SerDes Register bit fields manually?

Normally this is not required.

0 项奖励
回复