T2080 PVR Description

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 PVR Description

854 Views
scottgerhold
Contributor IV

In the T2080 Reference Manual, section 7.3.4.1 PVR mentions that the register is described in DCFG_CCSR_PVR (section 27.3.11). But the field descriptions don't match. In 7.3.4.1 it calls bits 24:27 the Processor Major Revision # and 27.3.1 calls bits 16-23 the major revision #. Which table is correct?

Labels (1)
0 Kudos
Reply
1 Reply

781 Views
ufedor
NXP Employee
NXP Employee

Both variants are applicable considering that Chapter 7 is named "e6500 Core Integration", so the "Processor" here means "Core":

MAJOR_REV = Process revision + Manufacturing revision

MINOR_REV = Processor (Core) major revision number + Processor (Core) minor revision number

0 Kudos
Reply